Part Number: TCAN3413 TI recommended to use the tcan33x.ibs file since the tcan34xx.ibs file fails parser checks. I downloaded tcan33xx.ibs. It does not have a differential input model to be used in simulation.
Part Number: TCAN3413 Other Parts Discussed in Thread: TCAN3403 , Hello team.
What are the differences between: TCAN3413 and TCAN3403?
Thank you.
Kind regards,
Wouter Kragt
Part Number: TCAN3413 Hi team,
I am looking into the TCAN3413, which is rated as Functional Safety-Capable, but I could not find any information regarding the FMD or pin FMA.. Are these data available somewhere?
Thank you
Part Number: TCAN3413 Here are the ERRORS reported for IBIS file tcan34.ibs by two parsers (Hyperlynx and Committee):
•tcan34xx.ibs(35) : Error : Declared differential pins CANL and CANH not previously defined for this component [TCAN]
•ERROR -
…
Part Number: TCAN3413
I just downloaded the IBS file for CAN bus buffer part TCAN3413DR from the TI.com website. It fails the IBS parser check and here is the log:
IBISCHK7 V7.2.0
Checking
NOTE (line 122) - Pulldown Minimum data is non-monotonic…
Part Number: TCAN3413 Tool/software: Hi team,
can you help to see if the TCAN3413 support below application? or do we have relevant device to support the transceiver function?
Part Number: TCAN3413 Tool/software: Hi,
I would like to use TCAN3413 interface in harsh EMC environment, but I cannot find any recommendation of CM Choke, which does not affect the CAN_FD performances.
Could you give me a recommended CM Choke…