Part Number: TCAN337 Other Parts Discussed in Thread: SN65HVD232 , , TCAN4550 , TCAN334 , TCAN1043 Hi Team,
Do we have Q1 version about CAN which only need 3.3V supply?
I saw TCAN33x ,but just industrial version
Part Number: TCAN4550 Other Parts Discussed in Thread: AM3352 Tool/software: Linux Hi SIr
We have referred to the Linux driver code TI offered and have some questions as below
PS: We used AM3352 platform and want to integrate TCAN4550 IC
Q1: It is necessary…
Hello Risto,
Thank you for your inquiry.
I've conferred with the digital designer on our TCAN4550-Q1 device. You should be able to read both header and payload information for a single or multiple received messages with one SPI transaction. However…
Other Parts Discussed in Thread: TCAN4550-Q1 Tool/software: Code Composer Studio Hello. I'm working on a project right now. I am currently working on a project to test the TCAN4550-Q1 using the TMS570LC4X. One of the two boards is TX and the other board…
Part Number: TCAN1042HG-Q1 Other Parts Discussed in Thread: TCAN4550 Hello
As I see, TCAN1042x series did not integrated power supply, do you have below CAN solutions: Output 5V voltage with en/disable control,capable >250mA, support CAN FD,
Part Number: TCAN4550EVM Other Parts Discussed in Thread: TCAN4550 Hello
I'm using TCAN4550EVM to my board by wired connection.
and I'm trying Linux Driver code (starting with lastest version.. 5.12.xxx).
Linux code provides a bit timing calcurate…
Part Number: TCAN4550 Hi,
currently we are performing a compare test between TCAN4550 and competitor's MCP2517FD-H/JHA + MCP2542WFDT-E/MF combination.
Both, TCAN and MCP are connected on the same CAN BUS. We have noticed something very strange, if…
Part Number: TCAN1051GV-Q1 Other Parts Discussed in Thread: TCAN4550-Q1 , TCAN1051 Hi,
My customer has designed in the TCAN1051GVDRQ1 and has a couple of questions coming out of reading the SLOA101b - TI CAN application note.
Would you be able to help with…