Part Number: TDP0604 Hi Team,
Hope you're doing well.
My customer HYC (leading T&M supplier) is developing the multiple screen testers. And they ask if TI have the 1:n buffers to duplicate the input DP signal to several (2,4,8.....) output signals…
Part Number: TDP158 Other Parts Discussed in Thread: TDP0604 , Dear Technical Support Team,
What's the difference between TDP158 and TDP0604 ?
I'd like to use DDI to HDMI2.0b with 10b formats.
Best Regards,
ttd
Part Number: TDP0604 Hi Team,
Do we have any product which can support input port interface(PCIe 3.0) and output interface(HDMI+LVDS)? Thanks.
Best,
Stanley
Hi Jeffrey,
The TDP0604 works better in a source applications. I recommend placing the part where it can compensate for the pre-channel optimally. The TDP0604 can do up to 12dB at a 3Ghz (6Gbps). I recommend placing the TDP0604 approximately 10dB of insertion…
Hi,
For U4004 I recommend swapping over to TDP0604.
For U4005 make sure that the SOC is able to handle DC coupled HDMI. If the SOC is not able to handle DC coupled HDMI, I recommend swapping U4005 to TDP0604 as well.
Keep in mind that the TDP0604/…
Hi,
I would recommend using the DP159 re-timer or TDP0604 re-driver for this design.
The Intel DDI interface has to be configured as DP++ source. Please see below for the DP159 and TDP0604 EVM design as reference.
5187.DP159RSBEVM REV B1.pdf
HSDC125_001_Schematic…
Hi David,
thank you for the reply,
Can TDP0604/1204 achieve this? I see there is a input signal detection, seems we can detect the input signal by if the device is in standby mode
Thank you,
Charles
Part Number: SN65DP149 Other Parts Discussed in Thread: TDP158 , TDP0604 Hi Expert,
I'm looking for a TI solution that can replace NXP/PTN3366NSMP. Can you recommend it?
I think the similar one is SN65DP149. Are TDP158 and TDP0604 also suitable?
Thank…
Part Number: TDP1204
Tool/software:
Dear Sirs and Madams,
We are using a TDC1204 for level shifting between the GPU and the HDMI.
The SDA and SCL of HV_DDC are pulled up with 1.8k ohms at 5V.
The usage is as shown in the Simple Schematic, but there…