Part Number: THS3061 I have a concern with the THS3061 I am using in one of my designs. In doing a bring up testing, I've noticed that the device preceding the THS3061, actually put out 3.1V into pin 5 of the THS. The THS was not biased at all and I actually…
Part Number: THS3091 Other Parts Discussed in Thread: THS3061 , , THS3491 I'm considering using the THS3091 or THS3061.
How do these two parts compare in regards to intermodulation distortion?
Is there a model/simulator that would allow simulation…
Part Number: THS3061 Other Parts Discussed in Thread: THS3062 , , OPA695
I'm looking at using the THS3061 op-amp (and by extension, possibly the THS3062 op-amp) as part of a simple circuit to add and subtract voltages. These voltages are small-signal voltages…
Part Number: THS3061 Other Parts Discussed in Thread: THS3491 , THS3062 When I run my simulation, the output at vout is incorrect. It appears to be a bandwidth issue (input sinewave is at 13.56MHz), but I don't understand why. If I configure the diff-amp…
Part Number: THS3061 Other Parts Discussed in Thread: THS3062 Hello Team,
Is there a dual alternative to ther THS3061DGNRG4 amp? I see there is the THS3062 but its marked for NRND so im hoping there is another amplifier family that i can consider.
Part Number: THS3061 Other Parts Discussed in Thread: OPA172 , THS3062 Dear TI expert,
Below is my schematic. I want to use THS3061 to generate output voltage Vo=10*V2-5, where V2 is between 0V and 1V. At present I use THS3061 as voltage-follower to…
Part Number: THS3061 Other Parts Discussed in Thread: THS3062 , Dear teams,
THS3061 is a single amplifier, and THS3062 is a dual amplifier. Their electrical characteristics are almost the same. But their CMRR plot are dramatically different, Fig 31 on Page…
Part Number: THS3061 Other Parts Discussed in Thread: THS3491 Hi Sir
We are going to design buck circuit by discrete solution.
For compensator part of high frequency power(10~20MHz) , does TI have any OPA for this kind of application ?
Or large bandwidth…
Part Number: THS3491 Other Parts Discussed in Thread: THS3061 , slew rate of THS3491 is 8000 V/us ((20% – 80%) and slew rate of THS3061 is 7000 V/us for 20V-step and 5700 V/us for 10V-step (25% to 75% level) which indicates that THS3491's rise time…
Part Number: THS3061 Dear Technical Support Team,
Datasheet shows decoupling below.
My circuit has two 0.1-μF in parallel for power supply(Vs).
Should I change from 0.1-μF to 6.8-μF ?
I think that PSRR is not good when noise frequency is high, so…