Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: THS3091 Other Parts Discussed in Thread: THS3061 , , THS3491 , TINA-TI Good day,
Busy with a design to use THS versions of IC, I come across contradiction in the data sheet
On hand have the THS3091 and the THS3061, real live measuring and comparing…
Hi Yatao, my simulation shows that you have -11.85V at the input of THS3121. This violates the common mode input voltage range of THS3121! Stay 3V away from the rails at the input THS3121.
And you drive the output of THS3061 into saturation. Your circuit…
Other Parts Discussed in Thread: LM7171 , THS6212 , LM6171 , OPA695 , THS3061 , THS3001 , LMH6702 , THS3091 , OPA694 Hello, I was wondering if anyone could recommend a replacement device for the Comlinear CLC300A. Thank you for any help. Regards, Joe
Part Number: TPA6120A2 Other Parts Discussed in Thread: OPA140 , THS3061 Hi
I intend to use the TPA6120A2 to drive a AKG K301 headphone (120Ohms impedance) but want sufficient drive to also connect lower impedance headphones.
I am not a fan of AC coupling…
Part Number: THS3202 Other Parts Discussed in Thread: THS3201 , THS3091 , THS3061 , LMH6702 Hi TI, I've noticed that the THS3201 and the double variant THS3202 are not recommended for new designs.
Are you planning to release an opamp with comparable…
Sali,
BTW the THS3061 and THS3091 both have slew-rates of 700V/us and can operate on +/-15V supplies. It does look like you really aren't using the negative side of the supplies. Is that correct? We can skew the supplies to say +25V/-5V in case you need…
Other Parts Discussed in Thread: THS3061 , OPA847 , THS3091 , LMH6702 , TINA-TI I'm trying to develop a QCM (quartz crystal microbalance) measurement system to drive a special 5MHz quartz crystal on it's overtones to track it's resonance frequencies. I'm using…
Other Parts Discussed in Thread: LM6172 , THS3122 , THS3062 , THS3061 , THS3091 , THS3092 , THS3096 , THS3095 Hello,
I have designed a circuit based on the LM6172. Now I am running in some problems.
Abnormal distortion of the signal above 10MHz sine wave input…
Hello Hooman
I thought so. Thanks for verifying. Does that imply one cap per each op amp?
This is the first I've heard of this design addition, so does 2nd harmonic distortion apply to all frequencies of the operating range or to only higher ones like…
Other Parts Discussed in Thread: TLE2071 , THS3061 , OPA1611 , INA163 Can plastic package op amps be IR re-flow soldered? If so, does TI publish a safe re-flow curve? I've seen many papers in the TI library on methods, techniques, tools etc., but can not…