Part Number: THS3470 I am using a Rev. B chip in a 10 MHz, +/-25V application. So far, it is working well. However, the DIE_TEMP output is not working. With no load, the output is static at ~1.8V, no matter the temperature. VMID and VDD are stable at…
Part Number: THS3470 Tool/software: Hello,
could you please tell me what is the roadmap for THS3470? When it will be released and available? I'm considering this OPAMP for our project. But I need more pieces to test and EVM is limited only for 1.
…
Part Number: THS3470 Tool/software: To the TI team:
We have purchased several of your THS3470REBEVM boards. We have the following questions:
1). When will the THS3470 part be finally released in production silicon and be able to be purchased? We have…
Part Number: THS3470 Other Parts Discussed in Thread: THS3120 Tool/software: Hi,
In the figure on page 12 of the datasheet, R FB_TRACE is shown in the V out path. However, the parameter section (page 6) defines R FB_TRACE as "Internal trace resistance…
Part Number: THS3470 Other Parts Discussed in Thread: THS3491 , BUF634A , LM7171 , Hello,
I need to design an output stage which has to generate a square and sine wave signal of 30Vpp into 100 Ohms. The square wave should be as boxy as possible of course…
Part Number: THS3470 Tool/software: We have evaluated the THS3470 on the evaluation board THS3470EVM. Setup: OPV was powered with +-30, current limited to 2A. Output voltage was 50Vpp. Output was connect with 1m RG58 cable to Lecroy Oscilloscope with…
Part Number: THS3470 Other Parts Discussed in Thread: ISOM8710 , ISO7710 Tool/software: I have a 3.3 V, 10 MHz square wave output from my in-circuit FPGA. I need to convert this signal into a sine wave, isolate it from my digital ground, and transmit…