Part Number: THS3491 Hi!
The THS3491 is amazing! I tested a few such op-amps a few weeks ago. The preproduction version XTHS3491IRGTR.
I would love to order about 50 more for my PhD-project.
Is there a chance to order more op-amps of the preproduction…
Part Number: THS3491 Other Parts Discussed in Thread: THS3095 , THS3091 Dear Technical Support Team,
Do you provide spice model ? I couldn't find it on web site.
http://www.ti.com/product/THS3491/toolssoftware
Its status is preview, so if you have…
Part Number: THS3491 Customer needs RoHS (Eco plan), Lead Ball finish, and MSL for this device, could someone please let us know what the projected statuses are?
Thanks,
Part Number: TIDA-060033 Other Parts Discussed in Thread: THS3491 Tool/software: Hi i want to get hold of a THS3491 bootstrap reference design board TIDA-060033. I see design details in your app note, I see photos of the board but no link or details of…
Part Number: OPA692 Other Parts Discussed in Thread: THS3491 Tool/software: Technical Support,
I'm considering using the OPA692 to split a pulsed signal, into two equal signals. However the supplies will be: 0 and 12V and the output pulsed signals are…
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 Tool/software: Hi Team,
My customer build a circuit using the THS3001 however the waveforme is different. the differences are only LOT accourding to cusomter.
Can you advise why the differences…
Part Number: BUF634A Other Parts Discussed in Thread: THS3491 , THS3091 , Tool/software: Hi,
I need an amplifier with output amplitude of 16 Vp-p into a 50 ohm load. Bandwidth up to 100 MHz, rise/fall time of 6 ns.
Could I use THS3091 or THS3491 as…
Part Number: BUF634A Other Parts Discussed in Thread: THS3491 , THS3470 Tool/software: The BUF634A can be used to drive many typical headsets used for home/commercial use.
Aircraft headsets though use 150/300/600 ohms plus Military use 8 ohms.
The…
Part Number: DAC38J82 Other Parts Discussed in Thread: THS3217 , THS3491 , THS4509 , LMH6401 , , LMH5401 , Tool/software: Hello
In our application, the output of the above DAC should go through a signal chain which allows us to do:
1. Image filtering…
Part Number: OPA810 Other Parts Discussed in Thread: THS3491 Tool/software: 1. how to use a operational amplifier to create a negative capacitance values with frequency response with 20Mhz