Part Number: THS4022 VGA_SPLITTER SCHEMATIC .pdf VGA SPLITTER_TOP PLACEMENT.pdf VGA SPLITTER_BOTTOM PLACEMENT.pdf
Hello sir
We are using THS4022ID Op-amp in of my project. Here we are splitting one VGA input to Two VGA outputs ( Using THS4022ID…
Other Parts Discussed in Thread: THS4022 , OPA857 , LMH6629 , OPA657 , OPA847 Hi, I am searching for a High Speed Transimpedance Amplifier.
I've tried to use the THS4022 connected as a transimpedance amplifier but he doesnt seems to be stabel like this…
Other Parts Discussed in Thread: THS4022 Hi,
There is a mistake on the dataheet of this product: THS4022 High-speed operational amplifier.
At page 1-4, R5 is 49.9 Ohm and not 49.9 kOhm as drawn
Have a nice day
W.D
Other Parts Discussed in Thread: THS4022 I would like to know how to use the THS4022 with a gain of less than 1. I have read the applications note "Using a Decompensated Op Amp for Improved Performance" (SLYT015 - May 2000) and if I understand correctly…
Part Number: OPA814 Other Parts Discussed in Thread: THS4012 , THS4022 Hi TIer
My customer use AD8034 (SOIC) in last design. They are looking forward to a new HSAMP to deal with more challenging input signal.
Customer do not want to change the layout…
Hi Sam,
3.6mA is pretty high input current, you can get away with a low gain (say 500ohms for ~2V max) , so you may not need the OPA855 to get the bandwidth numbers you need. Depends on the exact details of your pulse and the capacitance of the photodiode…
Part Number: THS3001 Other Parts Discussed in Thread: THS4022 , I have a device that has a THS 3002, well most likely a Knock-off as this device is not that old but based of an older design,
I have found the THS3002 but again it is a 'Knock-off' with…
Part Number: LM7171 Other Parts Discussed in Thread: THS4012 , THS4022 , LM6172 , OPA862 Hi Team,
A customer would like to design a single to differential stage using the LM7171 opamp. Since the LM7171 come in single channel package, how good is the…
Other Parts Discussed in Thread: THS4032 , THS4012 , THS4022 , THS4082 It seeems the tool does not work very much.
I need, for an audio output of a DAC an OPA with the followings
Double 8-Pin SOIC
Voltage feedback
Unity gain stable
rails >=…
" Wireline Data Transmission and Reception " by Xavier Ramus, describes a possible system architecture for transimitting a signal with high-frequency content over fixed line length. Also included are tables of some suggested TI high speed amplifiers for…