Part Number: THS4031 Greetings,
We are seeing a variance in noise performance of THS4031IDGNR physically marked:
first line "TI 57"
second line "ACN"
not legible but I believe third line is "327"
These parts are failing at almost 100%; they…
Part Number: THS4031 Hello everyone,
I currently have a problem with a THS4031 and a transformer. In short: I have an operational amplifier circuit and want to couple the signal (100kHz 10Vpp sine wave) somewhere else. The problem is independent of…
Part Number: THS4031 Tool/software: Hey team, can you help with the below?
I am attempting to document all the changes made in the datasheets for part THS4031 from revision SLOS224I to SLOS224L to see all changes made and see if any were retracted…
Part Number: THS4031 Tool/software: Regarding PCN 20240314000.1, the Differential Input Voltage has gone from +-4V to +-1.5V from Rev I to Rev L in the datasheet for part THS4031D.
Would you be able to help clarify the changes in voltages and if possible…
Part Number: THS4031 Other Parts Discussed in Thread: TLC7524 , THS3091 , THS3491 Tool/software: Hello, I need an alternative to THS4031ID with similar low settling time and low noise characteristics but with higher capacitive load drive capability. I…
Part Number: THS4031 Hi
Old chestnut about ensuring inputs are protected during power down conditions - is there a spec for the maximum safe input current?
My application: single supply; one input will see a reference of 3V filtered via a 1000uF cap…
Hello Alec,
Thank you for your reply. Today I tried reinport THS4031.lib and THS4031.olb files to OrCAD PSPICE library folder. And I executed setting of simulation profile to add THS4031.lib file and setting of design file to add THS4031.olb file. As…
Part Number: THS4031
Hello,
I executed PSpice circuit simulation to analyze stability for amplifier circuit used THS4031. The circuit is same circuit as figure 6 of application report SBAA135A. (Schematic for circuit simulation is shown below)
And…