Part Number: THS4052 Other Parts Discussed in Thread: TINA-TI Hello guys,
One of my customers is considering using THS4052 for their next products.
They want to know how much the device settling time in their assuming condition by TINA-TI.
Could you please…
Part Number: THS4052 Other Parts Discussed in Thread: TINA-TI , BUF602 , LMH6559 Hello guys,
One of my customers is considering using THS4052 for their new products.
They have the following questions about the device. Copuld you please give me your reply…
Part Number: THS4052 Other Parts Discussed in Thread: THS4631 Hello guys,
One of my customers is considering using THS4052 for a voltage follower. They have the following question about THS4052.
Q. Is 20 ohm resistor placed between THS4052 output and…
Part Number: THS4052 Other Parts Discussed in Thread: TINA-TI , OPA2810 Hello guys,
One of my customers is considering using THS4052 as a DAC output voltage follower for their new products.
For that, they want to measure output impedance of the device…
Part Number: THS4052 Hi,
how is the input resistance of the THS4052 specified? It is specified with 1MOhm, is this differential input resistance or is it input resistance as a non inverting amplifier?
Thanks
Other Parts Discussed in Thread: THS4052 , OPA2132 , OPA2277
Hello,
Please allow me to have a question in addition to other post.
In case using THS4052 for peak detector, and also in case input voltage were large ( 5Vpp; 10KHz ),
the large bias current …
Other Parts Discussed in Thread: THS4052 , OPA2312 Hello
My customer intends to use THS4052 for peak detector.
Anyway , if the input signal is large, the input signal has distortion.... attached Fig1
In case amp were OPA2312, it works well .
We( customer…
Other Parts Discussed in Thread: THS4052 Hello
My customer intends to use THS7052 for their peak detect circuit.
However, if the input signal were large, ( almost 5Vp-p ... i.e. same range of differential
input voltage rang +/- 4V on D/S page 2 ) , it…
Hi Ravi,
Thanks for your quick response.
42 mA is for full operating condition means it includes temperature variation of 0 to 70 degrees.??
Also i was looking at THS4052. Below is the output current
will it good if I use THS4052.
Thanks & Regards,…