Part Number: THS4130 Hello, The THS4130IDGNR differential amplifier heats up to +50°C. The circuit does not oscillate. The diagram below is used, the RG and RF resistors are replaced by 390R. I also tested R206 and R209 = 20R.
NMT =Not mounted.
…
Part Number: THS4130 Tool/software: Hi:
Using THS4130, I found that if -5V is powered on first, it will couple to +5V, but not vice versa. What could be the reason?
Thanks!
Part Number: THS4130 Other Parts Discussed in Thread: THS2630 Tool/software:
in THS4130 datasheet, VICM is -4 to 4.5V typ with Vcc=±5V, so if we change Vcc=±10V, VICM value will enlarge or still be -4 to 4.5V?
Part Number: THS4130 Other Parts Discussed in Thread: ADS9219EVM , OPA320 Tool/software: Hello team,
What is the current consumption at Vocm pin? The customer would like to connect voltage reference output with this pin. So, wants to double confirm…
Part Number: THS4130 Other Parts Discussed in Thread: THS2630 Tool/software: Could you confirm that the marki ng in the picture is THS4130CDGK? Thank you very much!
Part Number: THS4130 Tool/software: For THS4130lD, what's the allwable variance between VCC+ and VCC-. like, VCC+/- being ±10V,then what the allowable variance between abs of VCC+ and VCC-.
Part Number: THS4130 Other Parts Discussed in Thread: THS2630 Tool/software: Hello. I am looking to replace an obsolete PN THS4130IDGN, and the THS4130IDGNR looks like the best replacement. Are there any differences between these two part numbers? From…
Part Number: THS4130 HI I am Using THS4130 in my design with gain=20,and observed output harmonics are very high(-20dBc) request you to provide your inputs to increase the harmonics level
Attached schematic design for your review.
Part Number: THS4130 In SLOS318L the common-mode input voltage range is specified in section 7.5 Electrical Characteristics for a bipolar supply voltage of ±5 V as typically "–4 to 4.5".
What would be the minimum and typical common-mode input voltage…
Part Number: THS4130 I am developing a test adapter for testing OpAmps (DC parameters only )on the UNIMET / M3000 test station. Among other things, I chose the FDA TFS4130 to verify the device. For better verification, I lack more detailed test conditions…