Part Number: THS4131 Hi team,
My customer wants to purchase the small package version of THS4131, which package is MSOP or MSOP-PowerPAD. I saw the part numbers corresponding to these two package types on the revised datasheet.
However, when I tried to…
Part Number: THS4131 Other Parts Discussed in Thread: OPA1632
In the process of using THS4131, we found that if the feedback capacitor is 4.7nF and a DC input is provided at this time, an oscillation of 280/320MHz will be generated at the output end…
Part Number: THS4131 Hi Team,
Can you help diagnose the customer issue below?
A customer is testing the device using the schematic from the datasheet (see below).
In this test, the customer grounded both inputs instead of having a source voltage (a…
Part Number: ADS8412 Other Parts Discussed in Thread: THS4131 , ADS8422 , Hello,
I considering AD conversion circuit that circuit is used ADS8422 and THS4131. Current my schematic is besed on circuit of figure 29 of ADS8422 data sheet. However, current market…
Part Number: THS4131 Other Parts Discussed in Thread: TINA-TI Hi Team,
My customer would like to get 25db gain passing up to 10kHz input signal with THS4131 though, Is it achievable?
If yes, could you give me one of external components setting example…
Part Number: AMC3302 Other Parts Discussed in Thread: THS4131 , AMC3301 , Tool/software: Hi,
I need to measure the current up to 50A.
50A x 1mOhm = 50mV
50A x 5mOhm = 250mV
AMC3301 and AMC3302 both are fulfilling the requirement. After this, we need…
Part Number: THS4131 Other Parts Discussed in Thread: THS4141 , THS4151 Hi team,
My customer want to know if there is any performance difference between single rail power supply and dual rail power supply. Then I have some quick questions. 1. Could you…
Part Number: AMC1300B-Q1 Other Parts Discussed in Thread: THS4131 , AMC1300
Dear sir,
We are using AMC1300 for isolated voltage measurement and its output is connected to THS4131 amplifier.
THS4131 having +/-12V power supply.
+12V : Vcc+ of THS413…
Part Number: THS4131 Other Parts Discussed in Thread: ISO7710 , TLV9301 , TLV9302 , TLV9031 , TL331B , TLV1805 , TLV7211 Hello team,
Customer will use THS4131 with dual supply and PD function.
Power-Down mode requires the negative voltage to control at /PD…
Part Number: ADS1278-EP Other Parts Discussed in Thread: THS4131 , , ADS1278 , AMC1350 , ADS127L18 Tool/software: I'm trying to lay out a circuit using the ADS1278-EP driven with an isolated fully differential amplifier (FDA) to isolate the low-voltage section…