Part Number: THS4131 When configuring the THS4131 as depicted in Figure 30 in the THS4131 datasheet, we are able to see an amplified differential signal output with a gain of ~23, using resistor values Rg = 390 Ohms, Rf = 9 KOhms. When we place a second…
Part Number: THS2630 Other Parts Discussed in Thread: THS4131 , , TINA-TI I have a design that use the THS4131ID and this part is going obsolete and I am looking to replace it with new part THS2630 that is recommended on the THS4131 web page.
I have purchased…
Part Number: THS4131 Other Parts Discussed in Thread: ADS8422
hi every one i need to find out the total error at the output of Differential amplifier which is then fed in to ADC ADS8422.
input to diff amp is Vin + = 5.46 and Vin- =-2.73.
could you please…
Part Number: THS4131 Other Parts Discussed in Thread: OPA1632 Hello
What is difference between THS4131 and OPA1632?
I study both datasheets and can`t find differences.
Production control? THS4131 selected OPA1632?
-- Regards,
Victor
Part Number: THS4131 Hello,
My customer questioned what different between Thermal Information and Dissipation Ratings.
When I checked datasheet, based on D package, θJA is 97.5 and RθJA is 114.5. Why these are different?
Thank you.
Part Number: THS4131 Hi,
Simple, and maybe silly question: the data sheet for the THS4131 part shows a +/- 6V max input differential voltage (Table 7.1). I'm wondering if that's truly the case when operated with feedback and powered by +/- 15V rails?…
Part Number: ADS8422 Other Parts Discussed in Thread: TINA-TI , THS4131 , Tool/software: TINA-TI or Spice Models Hello
I am driving the ADS8422 with a THS4131 amp. My setup is fully differential.
The THS4131 is set up to give a high voltage gain of 7.5 …
Part Number: THS4131 Hello,
I am trying to figure out what would be the gain equation when the two feedback networks are different as bellow.
I my application Vs1 and Vs2 may differ slightly (~1%) and I am trying to ballance the amplifier. Rf1 and Rf2…
Part Number: THS4131 Other Parts Discussed in Thread: OPA2140 , THS4541 , TINA-TI I am troubleshooting a circuit with the THS4131. It is a new version of an old design where the THS4131 is also used and whose performance is OK. The problem is the original…
Part Number: THS4131 Other Parts Discussed in Thread: THS4130 , Is there any problem if I connect pin 7 to V+? That way I may use THS4130 in the same position (should I need it) without concerns about leaving PD pin open. I know PD may be left open but…