Other Parts Discussed in Thread: THS4502 Hi, Im simulating the THS5151 with multisim (the spice model from TI) and have some questions.
Why the positive and negative output have differents offsets (image of the simulation attached)? Can someone help me…
Hi Takashi,
No, there is no performance difference. If all node voltages in the circuit are shifted equally, the operation must be exactly the same. Voltage is just a measure of electrostatic potential between two points, and an amplifier will not know…
Other Parts Discussed in Thread: THS4151 Hi
I'm using THS4151 as a video differential driver. I use +-12V power supply.
CMV pin is used not to set reference voltage but to apply some ac signal.
CMV ac signal has 500kHz. but I found small portion…
Part Number: ADS54J40EVM Other Parts Discussed in Thread: THS4151 , ADS54J60 Hello,
We are using the ADS54J40EVM board to evaluate our design - Our board is connected to it.
1. We want to operate the board so the input will be Differential DC coupling.…
Other Parts Discussed in Thread: THS4151 Hi,
I have used the THS4151 op-amp to create a circuit that takes two inputs and subtract them to give an output. Below is the schematic for the circuit:
R1 is where I will input a 1 MHz, 2V sinusoidal signal,…
Part Number: THS6222 Other Parts Discussed in Thread: THS6012 , THS6022 , BUF634A , LME49724 , TINA-TI , THS4151 , THS4150 , THS4552 Hi, I am looking for a balanced output amplifier of a signal generator 0 - 300kHz, Vcc +/-16V, output total Rload 200R (between…
Hi,
We are unable to find THS4561for ordering in mouser /digikey. So we are proceeding with THS4151 model.
as suggested, created a new post with AMC1300 and THS4151. ( link )
Please check the circuit and share your suggestions.
Thanks &Regards, …
Part Number: AMC1300B-Q1 Other Parts Discussed in Thread: AMC1300 , THS4131 , Dear sir,
We are using AMC1300 based voltage and current measurement circuit. Please find the attached schematic and output waveforms.
Schematic.
The output waveform is
Channel…
Hi Kai-san,
thanks for your reply.
Yes, the orange curve has 2mV/Div. The differential output is acquired by oscilloscopes ch1 and ch2, and the difference is displayed by calculation.
Also they observed THS4151 for comparison. The time to set the output…
Other Parts Discussed in Thread: THS4151 , THS4150 I am going to be putting 3 THS4151 circuits on a board. Is there a minimum spacing I should maintain between them?