Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: THS4271 , THS4303 Hi,
I want to use THS4271 OPAMP with 5V Single Supply and AC Coupled.
The equivalent circuit of the source is signal source series with 8pF capacitor. I need 500kohm input resistance to reach my low frequency…
Oh I see now your schematic says THS4271, while your lead comment is the THS4275 - so no shutdown and reference pins.
To attach a file, use the paperclip symbol across the top
Part Number: THS3001 Other Parts Discussed in Thread: THS5671A , , LMH6723 , THS4271 , OPA695 , THS3215 , THS3217 , OPA837 I'm hoping to use the THS567EVM to convert from an FPGA output to custom analog input board, but we are using single supply (+5V) for…
Part Number: LMH6624 Other Parts Discussed in Thread: OPA843 , OPA694 , THS4271 , OPA659 We use an opamp to scale the DAC's output into a suitable voltage range. We're looking at using the LMH6624 at a gain of 3x. Apparently, there are some tricks…
Other Parts Discussed in Thread: THS4271 On-line manual for the module shows output resistor R6 = 453 ohms. Board I received has R6 = 100 ohms. Either board is stuffed wrong or documentation is incorrect. Which is it?
Thanks.
Part Number: THS4275 Other Parts Discussed in Thread: THS4271 , TINA-TI Hi,
I'm designing a photo-diode interface: Iout(diode)=~4mA, Fout=~40MHz, Cdiode=~5pF.
The output current from the diode in my case is relatively high so the required gain is rather…
Hi Hooman,
Thank you so much.
One question, the thermal pad on the LMH6629 is tied to the negative supply pin of the LMH6629. The data sheet for the THS4271 says to tie the thermal pad to ground. Were I to use the THS4271 in place of the LMH6629,…