Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: THS4303 , OPA855 Hello team,
Customer is trying to find THS4303 EVM schematic and layout files and I'm not finding it online or in previous E2E posts. Also as a side, is there a newer part we'd recommend instead of THS4303…
Part Number: THS4303 Other Parts Discussed in Thread: OPA692 , THS4304 Hi,
We are using THS4303 in one of our product as an amplifier to amplify the Oscillator output--But we are not able to see any output after THS4303.
The oscillator part number is …
Part Number: THS4303 My setup:
Using THS4303EVM with a Rigol DSA-815 Spectrum analyzer and Tracking generator (TG) sweeping from 1Mhz to 1.5 Ghz. The THS4303EVM input is connected to the TG and the output is connected to the spectrum analyzer input. The…
Part Number: THS4303 Hey there
I know from the datasheet, that the THS4303 powerdown cannot be used as an output tri-state function, but what is the S21 over frequency for the powerdown case? Unfortunately, the datasheet only gives numbers for the other…
Part Number: THS4303 Hi,
Can you please confirm the peak to peak output swing for the THS4303 amp with split +/-2.5V supplies? Looks like only the single supply swing is given in the datasheet
Thanks,
Anoop
Part Number: ADS4129 Other Parts Discussed in Thread: THS4303 , THS4541 , LMH6554 Hi,
Please find attached a snapshot of the ADC input drive circuitry I'm planning to use for for the ADS4129 ADC operating at 250MSPS Fs. In my application, my input signal…
Part Number: LMG1020 Other Parts Discussed in Thread: THS4303 , THS4302 , OPA858 , OPA855 Hello,
I'm looking for a TI amplifier that could boost a 1ns, 200mV pulse up to the required turn-on voltage at the IN+ pin of the LMG1020, assuming that the IN- pin…
Part Number: THS4303 Hi,
For my application, I find the performance specifications of THS4303 amp desirable, but I'd like to have an option to set the effective gain of the amp circuit to be 1V/V or 10V/V(which is the default fixed gain option). For this…
Part Number: THS4303 I am interested in use this op-amp for a Negitive Impedance Converter (NIC). I have removed the terminating R to gnd . Does the non-invert need a R to GND to operate. I do not get the expected results from the THS4303EVM, compared…
Other Parts Discussed in Thread: THS4303 Dear All,
I have one question on the feedback loop of THS4303.
I want use THS4303 to realize a negative inductor. The feedback loop between the output port and the Vin+ port of THS4303 consists of a capacitor and…