Part Number: THS4304-SP Other Parts Discussed in Thread: THS4304 , TINA-TI Hello,
I am trying to use THS4304-SP for one of my projects. So I downloaded the spice model for THS4304, however the spice model doesn’t work when I use single supply like 5V…
Part Number: THS4304-SP Hi team, working with a customer on this device. Some questions on the implementation of the device:
Datasheet on page 12 under General applications, discusses that 0.1uF ceramic cap is critical for power supply bypass. Text…
Part Number: THS4304-SP Other Parts Discussed in Thread: THS4304 I am using the THS4304-SP in an application where it is buffering/amplifying a ~10MHz sine wave reference clock. The ~10MHz oscillator may get powered prior to the supply for the THS4304…
Part Number: LMH6702QML-SP Other Parts Discussed in Thread: THS4304-SP Tool/software: I need to make a noise analysis for my application using the LMH6702QML-SP . I know that the total noise will the sum of the:
Voltage noise: The amplifier’s input…
Other Parts Discussed in Thread: THS4304-SP I wanted to confirm this quick question. THS4304-SP Rad-Tolerant Class V data sheet shows two Vout pin 6 &7. Should these outputs be tied together, or should only one pin be used? If the latter, which pin should…
Part Number: LMH6702QML-SP Other Parts Discussed in Thread: TLV3801 , LMH5401-SP , THS4304-SP , LMH5401 Tool/software: Hello,
My name is Pablo and I need to convert a highspeed 500MHz triagular signal into a 500MHz squared signal. I am thinking of using…
Hi Jenny,
As far as I know, TPSM846C24 module is not specifically manufactured to withstand radiation.
You may find some SEE TI products here: e2e.ti.com/.../slyt532g.pdf
Martin,
As I mentioned previously, we do not have such information. Our Modules are for commercial use therefore those tests are not performed.
I would recommend going to ti.com, click on top left corner "Applications" and select "Aerospace & defense…