Part Number: THS4503EVM Other Parts Discussed in Thread: THS4503 , THS4541 Hi,
I'm attempting to use the THS4503EVM in a non-inverting mode for a single to differential converter application.
I thought this would require simply removing R17, grounding…
Part Number: THS4503EVM Other Parts Discussed in Thread: THS4503 Hi
I wanted to achieve a gain of 10 by changing the feed back resistors to 1.3K and 118 Ohms as suggested. The input voltage maximum is 1V peak to peak @ 100MHz. I have done multiple test…
Hi Jesse,
Yes that should be fine. You can see a reference layout from the THS4503EVM users guide to use a reference. Smaller traces are used right near the part due to the pad pitch.
THS4503EVM User's Guide: www.ti.com/.../slou132.pdf
Regards…
Part Number: THS4503 Hi,
I used THS4503 in my board to convert a differential signal to a single ended one. I have used the same configuration as used in THS4503EVM, however, when no signal is connected the current consumption of THS4503 is almost…