Part Number: THS4511 I am using THS4511 with a simple resistive feedback as shown in the image.
As it was not giving me my desired gain according to my calculations. GBW=1600MHz, gain=24, leading to a bandwidth of 66MHz. But as seen from the image,…
Part Number: THS4511 Hi,
base on THS4511 DS, the utput voltage is 1.25 to 3.75V.
but the DS figure11 X axis show the Vcm form -1V to 1V.
how to understand the Vcm value? is the CM voltage be AC single?
Hello Jim,
The CFP HKT0016A package on those flight/space grade parts is unique to parts needing to meet the MIL-STD-1835 specification. Other than the related THS4513-SP part (also flight/space grade), no other TI FDA is sold in that package. The non…
Part Number: THS4511 Dear Sir/Madam,
I would like to find out the process technologies node for THS4511 - RGTT and SP.
Is both devices fab base on BiCOM 3 process technologies node.
What is the main different between RGTT and SP grade, is both…
Part Number: THS4511-SP Hi all,
1. Is there a gerber file available for the ceramic dual flatpack option available?
If not, what should be considered in layout?
The long leads will add additional inductance compared to the smt version.
/Mark
Hi,
The datasheet for the THS451-SP does not provide a minimum or maximum for open loop gain, only a typical value. Since this is only a typical value, the data post radiation would not have been captured.
The datasheet for the commercial version…
Other Parts Discussed in Thread: THS4511-SP , TINA-TI , THS4511 , ADS5500 On page 5 of the data sheet for the THS4511-SP it lists the max and min Quiescent Current. Is the Quiescent current draw the only current draw through the THS4511-SP? Is it correct…
Part Number: LMH6554 Other Parts Discussed in Thread: TIDA-00659 , LMH5401 , THS4511 , THS4509 Dear Sir/Madam, I have an application scenario involving small-signal amplification. I need to design a 4-stage cascaded CFB fully differential amplifier, with…
Part Number: THS4551 Other Parts Discussed in Thread: THP210 , THS4561 , THS4500 , THS4511 , THS4501
Hi team.
I am looking for an alternative part which has same specfications as THS4551, but should support for higher supply voltage range Minimum…
Hi Mochizuki,
While looking over the THS4511 datasheet in order to respond to your question, I found a potentially useful section on the applications of the THS4511. In particular, this section discusses the default common mode output of the THS4511…