Part Number: THS4521-HT Other Parts Discussed in Thread: THS4521 Hello TI team,
I am comparing the THS4521 and THS4521HD / THS4521‑HT devices and have a question about the difference in allowed supply voltage .
From the datasheets:
THS4521 (standard…
Part Number: THS4521-HT Other Parts Discussed in Thread: THS4521 Tool/software: Hello,
I'm using the THS4521 op-amp to sense current in my circuit. When I apply an isolated current supply (without powering the rest of the PCB), the differential output…
Part Number: TMS320F28379D Other Parts Discussed in Thread: THS4521 , , TINA-TI Tool/software: Here is a brief summary of my current work and the issue I’m encountering: ere is a brief summary of what I am doing:
System Setup: I am working on a…
Part Number: THS4521-HT
I'm using a THS4521-HT with a single 3.3V supply. I'm happy with an output common mode of 1.65V, is there any advantage of driving the Vocm pin with a buffered 1.65v signal rather than simply leaving it unconnected?
Kind…
Part Number: THS4521-HT Other Parts Discussed in Thread: THS4541 , THS4521 , THS4551 , THS4561 Hi There
I'm using a THS4521-HT running off a unipolar 0-3.3V rail
There's a user case where the THS4521-HT could see a +/-12V signal on one of its inputs…
Part Number: THS4521-HT Other Parts Discussed in Thread: THS4521 , Hi Team,
The powersupply of THS4521 is having max supply of +5V but THS4521-HT/KGD is having only +3.3V. Can you please help with reason for degradation of operating supply.
Regards…
Part Number: THS4521-HT Hi,
We are using -55 to 175 Deg C part and the input offset voltage should be within +-5mV. Though we are getting almost 9-11mV offset voltage from this part.
Can you please comment on this?
Part Number: THS4521-HT Other Parts Discussed in Thread: THS4521 The problem is that the output bias of ths4521 shkj is obviously larger than that of other normal ths4521 shkj chips when power is on. At the same time, the output of unstable ths4521 shkj…
And also Amar,
I was kind of wondering if there was any efforts to refresh the HT products. I did find a 2009 harsh environments guide, but this link is more recent - I did not look at it, but it might help you - the obvious question (to me) is if the…
Part Number: THS4521-HT Other Parts Discussed in Thread: TINA-TI , ADS1278 , , THS4521 , THS4551 , TL072 , THS4521EVM Tool/software: TINA-TI or Spice Models Hi There
I have a low frequency (say 10Hz) differential input signal coming from a sensor centred…