Part Number: THS4522 I am using the THS4522 differential amplifier in a transimpedance configuration. In the system it is in, there are conditions where the source driving the THS4522 may be powered up before the amplifier. In that condition, there will…
Part Number: THS4522 Other Parts Discussed in Thread: THS4552 , Tool/software: hello,
Can THS4552 replace THS4522?What are the differences between them?Are there any better full-differential amplifiers available?
Part Number: THS4522 The datasheet states that the outputs are sensitive to parasitic capacitance. I am running the THS4522 as a 2. order MFB low pass filter. Is this sensitivity true for my configuration as well?
Part Number: THS4522 Other Parts Discussed in Thread: THS4521 , THS4551 Hi,
I am trying to simulate a new design using LTSpice.
I downloaded the Spice model as a zip (sbom343e.zip) file from the TI website.
I am using ths4521.lib from the zip…
Hello Will,
"I interpret this as saying that Vin± can be from (VS-)-0.7 to (VS+)+0.7V, but the difference between the two can only be a maximum of 1V. Is that correct?"
This assumption is correct. No there isn't a nominal spec for the differential…
Part Number: THS4522 Other Parts Discussed in Thread: ADC3444 , , ADC3441 , THS4541 , THS4552 , TMUX1109 , TMUX1119 , OPA2381 , TINA-TI Dear,
My current design uses a THS4522 which drives the inputs of a ADC3441. I would like to increase the sample…
Part Number: THS4522 Other Parts Discussed in Thread: THS4552 , THS4551 Hi,
I suffer massive thermal drift on THS4522 used as a current shunt (1mR) amplifier to 25msps ADC.
it has 22x amplification factor (1k in, 22k FB). And designed bandwidth…
Part Number: THS4522 Other Parts Discussed in Thread: TMS320F28335 , THS4509
dear All,
i want to interface the THS4522 ( fully differential ) to a single ended ADC. i have 2 questions:
1) i need a circuit interfacing THS4522 to a single ended ADC…
Part Number: THS4522 Dear;
Please help to analysis this high pass filter with THS4522, it doesn't simulate successfully, and doesn't have bode diagram during AC transfer characteristic with TINA. 4336.4k.TSC
Thank you very much
Best regards
K…
Hello all! Thank you for your feedback. It is easy to go down the rabbit hole for TVS literature! I am still trying to evaluate options and determine the correct way forward.
I wanted to add some clarification. Between the two input pins of the THS4522…