Part Number: THS4531A Tool/software: Hello,
In Op-amps and FDAs, the output voltages ard affected by input off voltage and input bias current.
1) Is the output voltage produced by Vos and IB an AC voltage or a DC voltage?
2) Are Vos and IB…
Part Number: THS4531A Tool/software: I am re-d esigning a So ftware de fined r adio f or a 100kHz si gnal. I h ave sim ulated my An alog f ront e nd in T INA s ince I am u sing a TI O PAMP a nd t he sim ulation is acc eptable. Ho wever T he P CB I de…
Part Number: THS4531A Hi Team,
We would like to ask your help regarding our customer's inquiry below.
How do you setup device pins to measure CMRR.
What is the two values of common mode input voltage which are used to test CMRR to get typical value…
Part Number: THS4531A Other Parts Discussed in Thread: AMC1210 , , AMC1202 , THS4531 , THS4551 , TINA-TI Hi team,
Due to customer use ADBT1001 and current sense function. customer wants to isolate the current signal.
Can I use THS4531A to attenuate…
Part Number: THS4531A Hi,
Good Day.
What is PSRR on device THS4531AIDGK? Is this the output change per change on supply voltages from 2.7V to 5V? Or Not.
Please consider also checking figures 19 and 52 which listed PSRR in two ways as if each PSRR…
Part Number: THS4531A Other Parts Discussed in Thread: THS4531 , Hi, Good day. Our customer would like to know the difference between the THS4531A and THS4531. Can you please share the information with us? Thank you and stay safe. Regards, Cedrick
Part Number: THS4531A Other Parts Discussed in Thread: THS4531
We have tested the following circuit for evaluate the THS4531AID (SOIC8) as interface ( attenuator and single ended to differential converter ) for an ADC with differential input
As…
Part Number: THS4531A Other Parts Discussed in Thread: ADS127L01 , , THS4531 , OPA320 Please find THS4531A & ADS127L01 schematic snippet attached.
Using 10kHz test signal applied to PREAMP_P, PREAMP_M is set to GND, at C155 I see proper signal, but…
Part Number: THS4531 Other Parts Discussed in Thread: , THS4551 Looking at the parametric table THS4531 and THS4531A look to have very minor differences. Are these drip in replacements to each other? Are there functional differences?
Thanks,
TJ
Part Number: THS4531A
Hello everyone,
Whats the real current consumption of this IC in operation?
Simulating a circuit on TINA, the current consumption is 19mA. On datasheet the current consumption is 0.25mA.
Regards,
Leonardo