Part Number: THS4541 Other Parts Discussed in Thread: ADC3664 , Dear Team, In my project I have to design a front end for ADC3664. Here I am mentioning the input specifications. Input signal Amplitude:: Bipolar: -1.6 to +1.6V pulse width: 50ns I am planning…
Part Number: THS4541-Q1 Other Parts Discussed in Thread: THS4541 Hello Sir,
One of my customers is using below link to output THS4541QRGTRQ1 package information. But there is a error of this information and this issue causes a big failure during my…
Part Number: THS4541-Q1 Hello experts, In the datasheet of the THS4541-Q1 device there are two options of the PACKAGE OUTLINE - RGT0016A & RGT0016H. It seems that the RGT0016H is les relevant for the THS4541QRGTRQ1 & THS4541QWRGTRQ1. Could you pls advise…
Part Number: THS4541 Hi Team,
Customer have a THS4541IRGTR working abnormally. The phenomenon is that the impedance between the FB+ pin and the OUT+ pin increases significantly. Under normal circumstances, the impedance between the two pins is 8Ω when…
Part Number: THS4541 Other Parts Discussed in Thread: THS4520 Hello,
Originally RD used THS4541 for differential Amp after TIA, RD changed solution to LTC6404-4.
RD highlights that LTC6404-4 is included low pass filter.
RD looks for high bandwidth…
Part Number: THS4541 Hi,
Myself Felix, working as Functional Safety Engineer in Velodyne.
Could you please support for below topic ?
- Whether THS4541QRGTRQ1 is capable for ASIL B (D) automotive product ?
To be more precise “If I am having…
Part Number: THS4541
Hi Team,
Good day! I am posting this in behalf of the customer.
I have shared the full details of the inquiry here:
I am using THS4541 differential amplifier to amplify a very low-voltage signal. The max. achieved gain of…
Hey Josh,
You are correct that zero drift (or chopper) amplifiers eliminate drift (and 1/f noise!) but they are limited to approx less than 10MHz GBP - so no, there are no options like that for you
IF you included a ckt, I do could more - TINA file…
Part Number: THS4541-Q1 Other Parts Discussed in Thread: THS4531 , TINA-TI , THS4531A Hello,
THS4541-Q1 datasheet says: input common mode Vs-1.2V
Vs=3.3V so I would expect a Vin_cm max of 2.1V
I simulated it with a similar part number THS4531…