Part Number: THS5671A Hey team,
I have a customer who came to me with the below issue. Let me know if you have any thoughts to kick off this conversation.
"We are having a strange issue with THS5671A chip. I hope you can assist with it. Another group…
Part Number: THS5671A For testing the dac we are giving sin wave input (3mhz) and the sampling clock 46mhz from fpga. The input is exactly sin wave we have checked in matlab. We connected the mode pin to ground, so we are giving inputs as offset binary…
Part Number: THS5671A Greetings,
is this part THS5671AIPW have Pspice model file.
Can you please share it to me?
sfgvip126@hotmail.com
Thank u.
Regards,
Part Number: THS5671A Hi,
I am using THS5671 DAC in one of my projects.
Ii has current unbuffered output.I am converting it to a voltage by providing suitable termination 50/100 ohm. now i want any differential to single convertor using OPAMP.
Please…
In my experience the optimal performance is achieved with 20mA output current into an equivalent 50 ohm load. That is, with a 1Vpp signal swing (-0.5V to 0.5V).
Other Parts Discussed in Thread: THS5671A , ADS5484 , TPS74401 Hi out there,
THS5671A seems fine, but it hates step function.
(the lead-in of a sawtooth waveform)
Check this:
I think it is not a reflection, becouse that is this:
…
Hi Abhishek, the closet DAC we have is DAC2932 (12b, 2ch, 40MSPS) or THS5671A (14b, 1ch, 125MSPS) and both use a Parallel CMOS interface for the input data.
Part Number: THS3001 Other Parts Discussed in Thread: THS5671A , , LMH6723 , THS4271 , OPA695 , THS3215 , THS3217 , OPA837 I'm hoping to use the THS567EVM to convert from an FPGA output to custom analog input board, but we are using single supply (+5V…
Hi Jim,
Thanks for offering to take measurements for me, but rather than have you spend time on that, it looks like I may be better off using the THS5671A instead, since that appears to be designed for VD=3.3, VA=5 operation.
I was intending to…