Part Number: THS6204 Other Parts Discussed in Thread: THS6232 Tool/software: I need to drive differential line +/-10V
I need to receive differential line signal level +/-10V
Thank you
Part Number: THS6214 Other Parts Discussed in Thread: THS6204 , , THS6062 , THS7002 , THS6002 , THS6301 , THS6302 , THS6222 , THS4561 , THS4551 , THS4541 , OPA2863A , OPA863 , OPA2863 , OPA810 Hi TI Team,
I search the receiver that can match with THS6214…
Other Parts Discussed in Thread: THS6204 Why would a THS6204 configured exactly per figure 81 of the data sheet draw 100mA from +12V and -100mA from -12V with a 2V p-p 1MHz input?
Other Parts Discussed in Thread: THS6204 , THS3092 , THS3091 , THS3096 , THS3095 Can this device be treated as a quad amplifier?
In other words can I use the four amplifiers individually for independent functions rather than a dual differential line…
I am lookng for an appliactions document that better describes this IC and pin connections.
one specificly is Pin7 IADJ, there is no mention in the data sheet of how to best connect this pin.
is there a better detailed application doument or Evaluation…
Part Number: THS6301 Other Parts Discussed in Thread: THS6302 , OPA2673 , THS6214 , THS6204 , OPA2670 Hello,
we are trying to design a solution to convert VDSL2 to Ethernet.Profiles supported are - 8a, 8b, 8c, 8d, 12a, 12b, 17a, 30a
Can you help provide…
Other Parts Discussed in Thread: THS6204 , THS6214 Hi,
Is there any source for a spice model for THS6204 or THS6214?
Thanks a lot in advance for answering!
Regards, taabt
Other Parts Discussed in Thread: VCA824 , THS3091 , THS6204 , PGA870 , TLC7524 , TL074 , TINA-TI , LMH6554 , LMH6523 Hello,
I need to implement a variable voltage output amplifier....digitally controlled output voltage is ideal
the output needs…
Peter,
Yes, the fully differential amplifier architecture is capable of generating a well-balanced output from a single-ended input and I would expect better balance than the two op amp approach I showed before. Thus, a better approach than I had proposed…