Part Number: THS6222 Hi Team,
Posting on behalf of our customer.
Does the THS6222 CM buffer stay operational while the output is in shutdown? Or does the CM buffer shutdown also?
Regards,
Danilo
Part Number: THS6222
Tool/software:
Dear Teams,
Regarding PLC communication, the carrier frequency is set to 187.5kHz and the data communication rate is 9600.
The following is the electrical schematic diagram of the PLC part.
1.Please help to…
Part Number: THS6222 Other Parts Discussed in Thread: TMUX6222 Tool/software: Team,
There's a confusing about truth table.
In the diagram here, it looks like it's a NO state (Normally OPEN). It means when SEL1/2 is set "1", the SW is operated and…
Part Number: THS6222 Other Parts Discussed in Thread: TINA-TI Hi Team,
May I have your help on it?
My customer uses LTSpice and cannot use the TI pspice model but fails to use it!!!
Is there any normal version model file, not just only for TI PSPice…
Part Number: THS6222 Tool/software: Hi,
Could you let me know when THS6222 output is connected as parallel, what is expected issue?
Is there any damage issue?
Thanks.
Part Number: THS6222 Other Parts Discussed in Thread: THVD8000 , , THVD1500 , THS6232 Tool/software: Hi Team,
My customer is using THVD8000 and below are the achieved ranges -
Test case 1: on CAT6 cable which works for 1.2 Km
Test case 2: on Signalling…
Part Number: THS6222 Hi TI
Can THS6222 use single ended output,The customer actually tested that sending and receiving both use the same single ended design, which allows for normal sending and receiving. However, we are not sure if there are any potential…
Part Number: THS6222 Other Parts Discussed in Thread: THS6232 Tool/software: Hi team,
I received some questions about THS6222. Please support.
1. How do the D1 OUT pin and D2 OUT pin become Hi-Z in shutdown mode? Please tell me the architecture. …
Part Number: THS6222 Other Parts Discussed in Thread: THVD8000 , TIDA-010935 Is there similar part with 125degree amp?
application: Solar inverter
Regards
Brian