Part Number: THS7001 Other Parts Discussed in Thread: PGA870 , LMH6518 , JFE2140 , INA849 , PGA855 Hello TI,
I want to measure signal in range of hundreds of nV to hundreds of uV, the sensor is piezo disc which may or may not have DC offset, the signal…
Part Number: THS7001 Hi
I have problems and queries about this THS7001 chip. My specification is a gain of 18 dB. Here is the test set-up I used for your reference. When I tested and measured it, the gain is around 2 dB which didn’t meet the requirement…
Part Number: THS7001 Hello TI,
I am using THS7001 for single chip solution in my application, can i use pre- amplifier and PGA at a time ...?
what i need to set SHDN pin status when want to use BOTH PGA and Pre-Amplifier part ....?
thanks for…
Part Number: THS7001 Other Parts Discussed in Thread: LMC6482 , PGA113 , Hello TI,
I want to replace LMC6482 with PGA for Sensitivity adjustment
i already tested both PGA(THS7001 and PGA113) with my exiting Circuit, we not getting any solid solution…
For a typical Op-Amp design, I understand that I can just shift the voltage wherever I want. My concern with the THS7001 is that it has VCC+ VCC- and GND. I'm fine shifting VCC+ and VCC- around, but can I shift the GND? Or would I leave the GND connected…
Other Parts Discussed in Thread: THS7001 , LMH6502 Hello everybody. I have a question about the THS7001. The block diagram shows that there is a LPF on the output of the PGA part. However, the datasheet says nothing about the LPF's characteristics (e…
Part Number: THS4151 Other Parts Discussed in Thread: THS2630 , THS4131 , THS4130 , THS4150 , THS7001 Tool/software: We're planning on using a THS4151 in a new design, but are a bit worried since it is an older part. The THS2630 is listed as a drop-in…
Hi Sumeet,
This seems to be identical to the query in the thread below.
https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1359478/ths7001-ths7001
Best,
Raymond
Part Number: PGA855 Other Parts Discussed in Thread: ADS8900B , THS4551 , THS4541 , THS7001 , , LMH6629 , PGA870 Tool/software: We would like to use the PGA855 to directly drive an AD9653 16-bit ADC running at 20 MSPS. The maximum frequency of the signals…
Hello,
Unfortunately we do not have such a device within the precision PGA catalog. However, you may consider the THS7001, a high-speed PGA with gain from -22 to +20dB and small-signal bandwidth of up to 100 MHz.
Best regards,
Ian Williams Linear…