Part Number: THS7374 Hi team,
One of our customers is considering the use of the THS7374 for an EF signal camper block application.
Since the datasheet does not specify Noise Figure (NF) characteristics, we would like to confirm whether the THS7374…
Part Number: THS7374 Dear TI Engineer,
Our car camera uses NTSC analog signal with a resolution of 720 * 480. Due to the long communication line, we would like to add a signal amplifier, which only requires one CVBS. We are currently considering THS7374…
Part Number: THS7374 Other Parts Discussed in Thread: THS7314 , , OPA361-Q1 Hello expert,
My customer would like to find the replacement for ADA4432-1WBCPZ-R7. Would you like to provide the automotive grade solution to replace it? I checked another…
Part Number: THS7374 Other Parts Discussed in Thread: OPA875 , , OPA857 Tool/software: Hello Team
I am using two channels to pass video signals through THS7374IPWR. 75 ohm impedance matching, clear picture.
What chip (maybe video relay) can I use…
Part Number: THS7374 Tool/software: I'm trying to add a THS7374 to my video PCB design but it keeps failing in circuit.
The power supply is +5 VDC. I have a 1.1uF bypass capacitance across the supply: 100nF right next to the VS+ pin and 1.0uF right…
Part Number: THS7374 Hello -
I'm working on a design that utilizes the THS7374 with ac-coupled inputs and outputs to both CVBS and S-Video signals. The outputs will drive two separate sink devices, so I've utilized a connection on the outputs similar…
Part Number: THS7374 Hi team,
Customer has some questions
I intend on using THS7374 in a design (unless you can recommend a different part under $2).
My product contains two analog RGB outputs, which I'd like to mux into the final output. I plan…
Part Number: THS7374 Is there anything special that the customer needs to do to simply pass RS170 NTSC video directly through the device?
Do we have a schematic available that the customer could use that shows the components that need to be used if…
Other Parts Discussed in Thread: THS7374 Hi
I have use THS7374 , I have find a issue from bypass mode.
When I setting bypass pin on High ( use filter ) , The RGB signal Vlow = 0mV
but when I setting bypass pin on low (bypass mode) , The RGB signal…
Other Parts Discussed in Thread: THS7314 , THS7374 Hi Team,
There is a good new that we could DIN TI product!
Customer is looking for the replacement of ADA4432-1WBRJZ-R7
https://www.mouser.tw/datasheet/2/609/ADA4432-1_4433-1-878278.pdf
Please…