Denny,
We don`t have any code in the Processor SDK RTOS for this part to perform DDR ECC based tests but you can refer to the app note here:
7750.Build Robust System on KeyStone Devices.pdf
there are some test examples based on CSL that can be used…
Thank you Nikhil. I am checking internally in my team for the slave address.
Sharing following points and request to check and share :
1)
In the meantime , I am trying another way : Even this value is zero .
+static int palmas_rev_read(struct…
Hi, I don't have any peripherals plugged in. I tried to remove and reattach SOM but there is no difference. And you can find log files (SDK 8.0 & SDK 10.0) below.
U-Boot SPL 2021.01-g53e79d0e89 (Aug 04 2021 - 23:32:00 +0000)
Model: Texas Instruments…
Hello,
There are several TI online documents that can help you with understanding DDCs, and the GC5016
a) on the TI webpage under the GC5016 section - there is a free online GC5016 training seminar
b) GC Studio the TI software tool can be used…
Part Number: TDA4VM
Hi TI Expert:
Currently we want to verify Samsung LPDDR4 4GB 2nd source, UART fail log is "Timeout during frequency handshake".
How could we modify this issue??
Refer below same former issue:
TDA4 hang on uboot when uart…
Part Number: TDA4VEN-Q1 Other Parts Discussed in Thread: TDA4VL Tool/software: Hi, experts ,
I'm having problems debugging tda4ven's spl startup, I suspect a problem with the ddr initialisation. This ddr model I used before on tda4vl without problems…
Jamie Groeneweg said: but do you have a MibSPI manual for the closest chip that I have?
I thought I gave you the below TRM in my last reply. This TRM is for TMS470PVF24xB device which shares the same architecture as your device. The MibSPI chapter should…
Other Parts Discussed in Thread: TLV320AIC3204 Hi sir,
if ok, can suggest TI device to replace MAXIX device? thanks. MAX98300EWL+
MAX98300EVKIT+TDFN.pdf MAX9860
MAX9860.pdf
MAX98300EWL+
MAX9860