Randy,
Nice to know you did not observe the issue after setting it to 2. There is no such document for resetHDVICPEveryFrame. The brief info is in the h264encoder Userguide. You might have it. I have attached it here again. When it takes long time to…
Hi Emmanuel,
Thank you for the reply.
Can you please post in English going ahead.
I see a number of problems in your circuit which is the reason for the spike at the peak of current waveform. The SOC functions works properly. I have resimulated…
Response from applications:
Ringing and Thermals are two separate topics…
For the Thermals: he should take the copper shape and size he has for Vsw on the top layer and replicate it on all the layers, including the inner and bottom layer. He needs…
In addition, I saw the following content on page 95 of document:
/cfs-file/__key/communityserver-discussions-components-files/1023/mmWave_2D00_Radar_2D00_Interface_2D00_Control-_2800_10_2900_.pdf
However, some people in the forum say idle time cannot…
Kelong,
My apologies, I should have also included the condition for collecting raw ADC data.
To minimize your periodicity, you need to calculate the total chirping (active frame) time out of total frame periodicity, it should be less that total frame…
Hi Bernard,
Thanks for the support.
As suggested by you i have run the Webench and it gave me the design with UC1843J for my application which i am attaching here.
But i have a doubt that how come the Webench selected UC1843 for 18V-45V DC input…
I am currently working on interfacing a CY7C024AV-25AXI SRAM with an AM625 processor. I've successfully enumerated GPMC, but I need some guidance on the following:
Supported Modes for GPMC0 : Which mode supports interfacing a 4MB SRAM using CS2…
Hello,
Guy Mishol said: Regarding the "LE Power Class 1" - this feature refers to the transmit power classification. Device that supports this feature actually declares it can transmit up to 20dBm. I don't think it is related to the issue you described…