Part Number: INA700EVM Tool/software:
HI,
I need current sense Monitor module or EVM kindly suggest below Requirements.
Required 4 channels monitor each channels should have below specifications
1)Max current 10A
Voltages are +5v,-5V,+15V,-15V…
Hello John,
Here are my responses to your questions:
John B said: But both of them don't have isolator circuit to work negative power supply, right ? This need to add separately.
Correct, neither of these EVMs come with isolation. So, you can try…
Part Number: TMAG5170UEVM Other Parts Discussed in Thread: TMAG5170 , TI-SCB Tool/software: Hello,
I was able to get the TI-SCB board to work properly with the TMAG5170 A1 board. The GUI worked online but when I went to try the A2 board it did not seem…
Hello Rahul,
Can you check if this is happening to more than 1 device? This will help us narrow down if it's with the device itself, or with the specific setup/hardware/software. You could also try using our EVM's MCU ( https://www.ti.com/tool/TI-SCB…
Thanks Alicia, we have a couple of follow up questions:
1) Does TMAG3001, or any other TI TMAG product have source code to aid software development?{(All products have an EVM but only demo code with TI-SCB MSP430. We are hoping for the source code related…
Part Number: TMAG5170UEVM Other Parts Discussed in Thread: TI-SCB I am asking you because there is a problem in the process of sensor testing using the TMAG5170UEVM_GUI program by purchasing two TMAG5170UEVM boards and TI-SCB boards. One TMAG5170UEVM…
Hi Kenley,
MAG_CH_EN should not have to be set, I was just asking in case it was.
Using the same settings that you are with an analog discovery 2 kit, I was able to successfully read back the temperature data, so I am not sure why it doesn't seem…
Other Parts Discussed in Thread: MSP432E401Y , TI-SCB , TMAG3001EVM , TMAG3001 , MSP-EXP432E401Y Tool/software: I could see that the browser firmware flasher could detect the hardware for a few seconds and then it says: "ERROR: Connection to BULK device…
Hi Austin, Yes, the Sensor Control Board (SCB) and INA237 EVM can interface with an online plotting and data logging tool. Please see the links below for more information. The EVM user manual is very informative as well. https://www.ti.com/tool/INA228_237_238EVM…
Part Number: TMAG5170DEVM Other Parts Discussed in Thread: TI-SCB , Dear team,
We are using TMAG5170DEVM + TI-SCB and connect to win10(or win11) computer with its GUI(or web GUI). But the PC did not recognize it.
We have referred to the FAQ and tried…