Part Number: TIDA-00203 Tool/software: Code Composer Studio We have been running the CAN to Ethernet demo successfully on the TIDA-00203 web site. It always worked for us. We can ping the board at 169.254.254.255 (default IP for demo) and run the CAN demo…
Part Number: TIDA-00203 Hi,
I am using TIDA-00203 and trying to get the entire CAN frame in raw bits instead of the tCANMsgObject that's used by the CANMessageGet API. I am using TiVaWare_C_Series-2.1.3.156 driver library.
Does any one knows if it…
Other Parts Discussed in Thread: TIDA-00203 Hi,
I am working on an assembled board of the design TIDA-00203. I am trying to retrieve the entire CAN frame, including the header fields, the data field, and the trailer fields, and send it over to Ethernet…
Hi,
As a test to check my CAN signal coming into CAN0 of the TM4C was good I ran this test.....
I sent a character from the DK-TM4C123G onto CAN1 on the TIDA-00203 (which works). This works and I get a CAN1 interrupt and the character is displayed on…
Other Parts Discussed in Thread: TIDA-00203 Hello! I have some problem about Software Download.
I develop the ARM Processor Custom Board(CAN to Ethernet Convertor) to using the TIVA C Cortex M4.
Now hardware develop completely but test software not yet…
Other Parts Discussed in Thread: TIDA-00203 Hello,
I am a hardware Engineer and working on a project that needs to incorporate the functionalities of TIDA-00203. The board needs to comply with the EMI/EMC, Temperature, Humidity and Vibration qualifications…
Hello Ravin,
Thank you for the message.
Please check if the below links could help.
Please note that these are not for DP83820 but can be referenced is it helps.
https://www.ti.com/tool/TIDM-TM4C129XS2E
TIDA-00203
Have you consulted the processor vendor…
Part Number: DP83867IR Other Parts Discussed in Thread: TIDA-00203 , TIDA-00204 Hi all Would you mind if we ask DP83867IR? Do you have default register setting with RGMII as reference data? Or, if it possible and you have .c source code of TIDA-00203(EMI/EMC…
Hello Amit,
Did you receive an update on how I can program the 2x5 2mm header on the TIDA-00203 or do we need to solder up our own cable to the .05 spaced 2x5 cable on the Blackhawk USB 100.
We are using a twisted pair cable with 120 Ohm between CANH…