Part Number: TIDA-00207 Other Parts Discussed in Thread: STRIKE Hi team,
My customers are creating circuits based on TIDA-00207.
They are studying whether ESD protection element can be used as it is.
They request HBM 20kV or more in the system.…
Part Number: DP83848K Other Parts Discussed in Thread: TIDA-00207 According to the ETHERNET standard, clause 8.3.2.1. Isolation shall withstand at least one of the following electrical strength tests:
a) 1500 V rms at 50 Hz to 60 Hz for 60 s, applied…
Other Parts Discussed in Thread: TIDA-00207 , DP83848K Hi, I'd like to know about a TIDA-00207. www.ti.com/.../tida-00207
Is the TIDA-00207 board being passed the 10/100 Ethernet Compliance Test?
My customer has failed "Transmitter Return Loss…
Other Parts Discussed in Thread: TIDA-00207 , DP83630 Please advise if your reference design TIDA-00207 (EN55011 compliant, Industrial Temperature, 10/100MBps Ethernet PHY Brick Reference design) has been tested against the IEC standard for conducted…
Hello Jomon Thomas,
Thank you.
Refer below for implementation https://www.ti.com/tool/TIDA-00207
Can you please point me to the bulk capacitors for IOVDD3V3 supply
Regards,
Sreenivasa
Part Number: DP83848M Other Parts Discussed in Thread: TIDA-00207
Hello,
I am using the DP83488 in a design and I am currently selecting the crystal. In order to verify that the selected crystal operates in its permitable power range, I need to calculate…
Part Number: DP83848I Other Parts Discussed in Thread: TIDA-00207 Dear Aniruddha Khadye ,
I "finally" find your answer regarding why initial question on the DP83848I : https://e2e.ti.com/support/interface/f/138/t/812032?tisearch=e2e-sitesearch&keymatch…
Hi Ross, Thank you for your reply. I'm a little troubled. My customer is using DP83848K and they have already completed their custom board. Their schematic is the same as TIDA-00207. So, CMC is on the phy side. Because TI is providing TIDA-00207 as reference…
Hi FC,
We have a design and layout guide for Ethernet PHYs: http://www.ti.com/lit/an/snla079d/snla079d.pdf
I would recommend using that as a starting point to verify that all the necessary PHY requirements are met. There is also a reference design…