Part Number: TIDA-00289 Other Parts Discussed in Thread: DRV110 I have a question regarding the latch in TIDA-00289, specifically how the plunger movement detection circuit resets.
Much treatment is given to the operation of the plunger detection circuit…
Other Parts Discussed in Thread: TIDA-00289 Hello, i am trying to use this TI design TIDA-00289 for fast switching solenoid. It's switching time is 0.5 ms ON and 0.5 ms OFF with the maximum operating frequency is 1000hz. Is that possible to limit the output…
Hi Thomas,
as I'm aware of there might be one design with low-side drive in industrial sector.
Please check TIDA-00289 out.
Please let me know if this helps.
Kind regards,
Tomas
Part Number: DRV110 Other Parts Discussed in Thread: TIDA-00289 , DRV8873 Hi team,
My customer is using a solenoid in their application to provide vibration feedback.
I'm considering promoting DRV110 and TIDA-00289 to them. Do we have any automotive…
Hi John,
Reviewed your setup to which I have additional questions/suggestions that may solve your initial concerns:
Problem #1 - Unexpected IHOLD, also noisy. Want 16mA, getting 5mA
Problem #2 - CKEEP (TKEEP) = 80ms instead of expected 100ms
Could you…
shishod,
Check out TIDA-00289 . While this design is centered around DRV110, there is an example of the circuit you mention, and this TI design provides some walk through of solenoid characterization and how to characterize your solenoid's current curve…
Thanks. i'll check if it works or not with your suggestions?
Could you support the TIDA-00289 EVM to customer? It's an important project they are doing. If ok, i gonna to give you address in separated mail.
Regards
Brian
Part Number: TIDA-00284 Other Parts Discussed in Thread: TIDA-00289 , , TIDA-01250 Hello,
Application in our company's machines require a section of solenoids which are pushing an object against the transportation band during certain process (up to 80-90…
Other Parts Discussed in Thread: DRV110 , TIDA-00284 , TIDA-00289 Hello,
I have a question for TIDA-00284 Reference Design with DRV110.
As my understanding, the resistor connected to HOLD pin of DRV110 used to set I HOLD current, and the equation is 150mV…
Other Parts Discussed in Thread: TIDA-00289 hi,
I need to capture the middle peak of the current waveform as indicate in the green colour waveform below.This is the surge for the solenoid which happened within 2Mhz to < 10MHz.
I have look at the…