Part Number: TIDA-01021 Other Parts Discussed in Thread: LMX2594 , LMK04828 Hi,
In the document Multichannel JESD204B 15-GHz Clocking Reference Design (Rev. A) says:
" Because the LMX2594 devices are being used in master mode, SysRefReq signal needs…
TIDA-01021_Clocking_Board_Engineering_Change_note_2017_1219.docx Hi Mats,
It seems there is an issue of mismatch between the latest schematic and layout. Gerber and CAD files are not updated with the latest schematic and BOM. If you have fabricate the…
Part Number: TIDA-01021 Other Parts Discussed in Thread: LMK04828 , Hi TI,
When running the TIDA-01021 and trying to set the LMK04828 to produce a continuous SYSREF signal I run into problems. PLL1 is programmed to produce a 100MHz signal from a 100MHz…
Part Number: LMK04828 Other Parts Discussed in Thread: TIDA-01021 , LMX2594 Tool/software: TI C/C++ Compiler I assembled a card named TIDA-01021 which TI not saled for test the chip of lmk04828 and lmx2594 how to sync between boards,but I find the board…
Part Number: LMK04828 Other Parts Discussed in Thread: LMX2594 , TIDA-01021 Hi, all:
I have two questions about LMK04828B:
1. Could cascaded zero-delay or nested zero-delay all be used to realize a fixed deterministic phase relationship between all…
Part Number: LMK04828 Other Parts Discussed in Thread: TIDA-01021 , LMK61E2 , Hi, all:
I have a question about digital lock of PLL1 in the LMK04828B.
As below figure.1 shown, I supply a 10MHz from TCXO to CLKin1, Fpd is set to 10MHz, and external…
Part Number: LMX2594 Other Parts Discussed in Thread: TIDA-01021 , LMK61E2 , LMK00304 Hi,
I have a question about LMX2594. My setup is listed below which refer to TIDA-01021 design :
1. LMK61E2 output 100MHz to OSCin of LMK04828B
2. OSCout of LMK04828B…
Part Number: LMK04828 Other Parts Discussed in Thread: TIDA-01021 Hi,
My test setup as below figure shown, signal generator(E8257D) provide reference 10MHz clock to CLKin0 pin of respective LMK04828B on the different board through PD1, for common clock…
Part Number: LMK04828 Other Parts Discussed in Thread: TIDA-01021 , LMX2594 , , LMK00804B , LMK61E2 Hi,
I would like to use LMK04828B+LMK2594 to provide device clock(10GHz) and sysref(4.8828125Mhz) clock to 4pcs ADC at the same time, and realize multichannel…
Hi, Noel:
I have no enough bandwidth probe to test 10GHz output from LMX2594, so I calculated the phase change through observing the acquisited waveform from two ADC which are clocked from the two LMX2594 respectively, as below figure shown. when I…