Part Number: TIDA-010232 Other Parts Discussed in Thread: AMC3330 , TLV6001 Hi Ti,
I use Pspice to simulate reference design TIDA-010232 to calculate RisoP and RisoN, but answers are not correct.
Could you please give me a hand?
Please refer to the schematic…
Part Number: TPSI2140-Q1 Other Parts Discussed in Thread: TIDA-010232
Dear TI Team,
I'm currently reading the Design Guide: TIDA-010232 AFE for Insulation Monitoring in High-Voltage EV Charging and Solar Energy Reference Design. In this file, insulation…
Part Number: TPSI2140-Q1 Other Parts Discussed in Thread: TIDA-010232 , , TPSI2072-Q1 Hi,
Customer refer design Guide: TIDA-010232 to insulation Monitoring, they system voltage need 1500Vdc max, but the design is for 400Vdc system,
Do you have an idea…
Hi Seungmin,
Saleh Ahmad said: The AMC131M03 has an internal PGA. You can set the Gain to 128, which would make your full-scale input +-9.375mV. For +-30mA, a shunt value of ~0.31Ohms would be good (9.375mV / 30mA = 0.3125Ohm). I'm not sure what the power…
Part Number: TPSI2140-Q1 Other Parts Discussed in Thread: TIDA-01513 , TIDA-010232 Could you please share the details for the Simulation (spice model )for this TPSI2140-Q1. So it will helps us to simulate with all the extreme conditions.
Part Number: AMC3330-Q1 Other Parts Discussed in Thread: AMC3330 Hi all,
I have referred the insulation monitoring for DC load system with respect to chasis https://www.ti.com/tool/TIDA-010232
Our requirement is to measure the AC insulation system with…
Hello Ibrahim,
Thanks for reaching out to our team. I would recommend taking a look at another TI Design for insulation monitoring where there is more active support, TIDA-010232 .
Mohammed Ibrahim Saqib said: I would like to know if the ground referencing…
Part Number: TPSI2140-Q1 Other Parts Discussed in Thread: TIDA-010232 , , AMC3330 Hi TI,
I would like to know design tolerance of TIDA-010232 reference design.
I only know how to run a worst case with tolerance of resistor.
Is IC model set with typical…
Part Number: AMC3330-Q1 Other Parts Discussed in Thread: TIDA-010232 , AMC3330 , TINA-TI , PSPICE-FOR-TI Hi TI,
I would like to know design tolerance of TIDA-010232 reference design.
I only know how to run a worst case with tolerance of resistive bridge. …
Hello,
unfortunately we do not have any PCB anymore. As Ryan pointed out, we can only offer your customer build their own board using the Altium design files or the Gerber files to build their own PCB? s this still an option?
I'd also bring your attention…