Part Number: TIDA-010244 Tool/software: Hi Support Team,
Ia, Ib and Ic can be measured separately in TIDA-010244. In = -( Ia + Ib + Ic ). could you please let me know why the neutral measurement circuit is needed? thanks,
Part Number: TIDA-010244 Tool/software: Hi support team,
In Figrue 2-2, the HGND_C and HGND_C_FB are separated, but are connected in Figure 2-3. If they are connected together, what do the C58 and R73 play roles in the Figure 2-2? thanks,
Part Number: MSPM0G3519 Other Parts Discussed in Thread: MSPM0G3507 , SYSCONFIG , TIDA-010244 Tool/software: Hi Team,
My customer is moving project from G3507 to G3519, due to the errata on G3507.
while they are moving exist project, RTC has changed…
Other Parts Discussed in Thread: ADS131M08 , TMS320F280049C , TIDA-010244 , MSPM0G1519 , MSPM0G1507 , TIDA-010243 , MSPM0G1506 Tool/software: Hello,
I’m interested in using the ADS131M08 as a replacement for the MCP3914B on the PIC32CX2051MTC128 Development…
Hi Anitha,
There is no key storage on the MSP430 parts but on MSPM0 we do have key storage. The device linked in the post does have AES but no key storage.
I recommend looking at the MSPM0G3519 for the additional key storage secure boot. We have a…
Measurements are performed using three external 24-bit ADCs (ADS131M08), with a target accuracy of Class 0.1. Our architecture is based on the TIDA -010037 (or TIDA - 010244 /3) reference design, which also utilizes external ADCs and mentions harmonic calculations, though the order is not specified.
Hi Haydar,
Sorry for the delay.
HAYDAR BILHAN said:
We do not necessarily need the A/D conversion of the baseband signal at 3MHz, but rather the envelope or the RMS value of it.
This should work fine.
HAYDAR BILHAN said: We are concerned capacitive…