Part Number: TIDA-01130 Dear All,
I would like to use the TIDA-01130 camera module, but I have to access it through V4L2, so I need to create a driver for it.
The User Manual states that I sould refer to the OV2775 datasheet for the sensor initialization…
Part Number: DS90UB953-Q1 Other Parts Discussed in Thread: TIDA-01130 HI
Can TIDA-01130 be replaced with 935/936, achieve OV2775 open HDR mode.
http://www.ti.com/lit/ug/tidud51a/tidud51a.pdf
Part Number: TDA3 Hi,
I have started a new driver for the OV2311 in VSDK 3.3 and am heavily deriving from the OV2775 TIDA-01130.
Currently I have integrated the OV2311 Sensor register settings as given by another reference driver. The sensor I2C accesses…
Part Number: DS90UB953-Q1 Other Parts Discussed in Thread: TIDA-01130 HI Sir
I refer TIDA-01130 reference design
1. The XCLK is 0.0696V ,is it enough for OV2775?
2. I saw the minimum load is 35kohm ,but reference design is using 402ohm ,which one is correct…
Part Number: J721EXSOMXEVM Other Parts Discussed in Thread: TIDA-01130 , TDA4VM Hi,
We want to purchase the Fusion application Daughter board EVM577PFUSION-V1-0 and the camera board TIDA-01130, to test the camera system with J721E SOM + J7X Common processor…
Hello Eitan,
Please provide additional information as the the type of interface and design specifications. There are many implementations of PoC, so please provide more detail as to what this is to be used in conjunction with.
There are Reference Designs…
Nick,
I do not think there is any data specific to the TPS65721 that is available, but power for CMOS Image Sensors typically uses a cascaded Buck-->LDO topology.
You can review the test data from these designs to see the effect of an LDO (spec'd at…
Hi Max,
sorry the EVM board source is not public in website. You can check TIDesign on 953's refer. design.
www.ti.com/.../tida-01130
best regards,
Steven