Part Number: TIDA-01471 Other Parts Discussed in Thread: XTR111 , TLV431
Hi Texas,
I have implemented the attached circuit, and the voltages shown have been obtained. What is the error?.
VCC24 = 24V
AVDD = 3.3V
IEPE.docx
Thanks,
Hello,
I would suggest you to look into TIDA-01471 . This is also an IEPE vibration sensor Interface for PLC analog input reference design and you will find all the design files in the landing page.
Please let me know if this helps.
Thanks
Giovanni
Part Number: TIDA-010249 Other Parts Discussed in Thread: TIDA-01471 , ADS127L01 , THS4551 , OPA2320 , DAC80501 Dear,
Recently I am working on the IEPE Sensor analog front circuit, and found TIDA-010249 reference design was helpful. (TIDA-01471 reference…
Part Number: TIDA-01471 Hi!
I'd like to make TIDA-01471. And I downloaded gerber and other files.
But I didn't find NC drill file which is needed to make PCB.
Can you give me it?
Part Number: ADS1274 Other Parts Discussed in Thread: TIDA-01471 , , ADS1278EVM-PDK , ADS127L11 Hello,
I need to design an IEPE 4 Channels Adquisition data Board. The client set the following specifications:
- Frequency adquisition = 10KHz.
- Resolution…
HI Shibin,
As Kai has mentioned, on the current transmitter application, the main issue with the Howland Current source configuration is that could be sensitive to capacitive/inductive load and will likely become unstable while driving a long cable. There…
Part Number: ADS127L01 Other Parts Discussed in Thread: TIDA-01471 Dear Technical Support Team,
CCLD and IEPE are called differently, but are they the same? Can the circuit of TIDA-01471 be used for CCLD as it is? Please let me know if you have any concern…
Part Number: ADS127L01 Other Parts Discussed in Thread: TIDA-01471 , Hi,
I have any questions.
1. Please tell me the reason why R2, R3 and R4 described in "Schematic" of TIDA-01471 are connected.
https://www.ti.com/tool/TIDA-01471
If the reason…
Hi,
This is my first interaction with IEPE. I was looking at these two dev kit
https://www.ti.com/lit/ug/tiduem9/tiduem9.pdf?ts=1642780960869&ref_url=https%253A%252F%252Fwww.google.com%252F
www.ti.com/.../TIDA-01471
rather than designing these boards…
Other Parts Discussed in Thread: TIDA-01471 , THS4551 , XTR111 , THS4561 , THP210 Hi!
we are experimenting with predictive maintenance in the factory of our client, on lathe spindle bearings. The single axis accelerometer sensor we would like to use is CMSS…