Hi Felix,
We have a UART over BLE bridge example that may be helpful for you. This example takes in UART input and sends it via BLE to a companion device. It is also able to take BLE input and output it via UART as well. The example may be found here…
Hi Dan, You meant Rds(on) sensing using LG and SW-PGND (as drain -source pins), right? LMG2100R044 doesn't has gate pin exposed. But, we can use LI pin as gate pin with RC delay equivalent to propagation delay from LI to gate(33ns). Let me know if this…
William-san
Thank you for your support.
Our customer has additional questions.
(1) When will the block diagrams of the output stages in the datasheets be changed?
(2)Why do the SW characteristics not change even though the output stage configuration…
Part Number: TIDC-CC2530-CC2592EMK-RD Other Parts Discussed in Thread: CC2530 , CC2592 , CC2591 Hi all,
Currently I am using CC2530 and the CC2591 in a device (in production). I received a notification saying that CC2591 is not recommended for new design…
Part Number: UCC28180 Other Parts Discussed in Thread: UCC28065 , UCC28056 Tool/software: Hello team,
I assume CCM PFC has better in power loss(power dissipation) than CrCM PFC when overall conditions are the same(or similar) like : MOSFET Rds(on), Diode…
Part Number: TIDC-CC2530-CC2592EMK-RD Other Parts Discussed in Thread: CC2592 , CC2591 hello
I tested the CC2592 Device.
Range Extender Set the CC2592 : RSSI : -65dBm
Range Extender Set the CC2591 : RSSI : -54dBm
The difference between setting the CC2591…
Part Number: TIDC-CC2530-CC2592EMK-RD Other Parts Discussed in Thread: CC2530 , CC2592 Hello
I want a design review for an attachment.
and check the CC2530 GPIO for PA_EN/LNA_EN/HGM control.
I Request a software example code
zetmote1801_181228.pdf
Regards…
Part Number: LMG2100R044 Other Parts Discussed in Thread: LMG2100R026 , , LMG3100R044 , LMG3100R017 Tool/software: Hello,
I am trying to use the LMG2100R044/LMG2100R026 as a high side current switch for a high power load. I attached a picture of my design…
Part Number: TDA4VM-Q1
Tool/software:
Hi TI:
Please share Micron MT53E1G32D2FW-046 AIT:B DDRSS_RegConfigTool excel list, we want to update new LPDDR4 setting for DRAM issue. Our default DDRSS_RegConfigTool refers J721e STK default setting(MT53D), never…
Hello Nicholaus,
Sorry for delayed reply.
Actually I was trying different ways to make drive work but still I am not succeeded in that.
I took short length SATA cable 8" length but that not help.
Then I changed my USB 2.0 connection. I bypass USB…