Part Number: UCC24624 Hi,
Noted that UCC24614/ UCC24624 are made for 230V at maximum. This means it only rectifier <230V AC.... What if my AC is 1000V? What if my AC is 500kHz? Anything from TI product can help to make up compatible SR Controller?
Sincerely…
Hi Saleh
As per your suggestion, i made bit modification to circuit. I have done simulation and proof of concept for the following circuit, and I am getting the expected results. But I want to understand how the AC signal is amplifying in this circuit…
Part Number: PRUCAPE Hello TI team,
I have AC voltage source of 10V/400Hz. I want to control it's amplitude with the help of controller.
How can I do this?
Thanks & Regards,
Prakash
Part Number: TM4C129XNCZAD
Hello,
Currently I a close to finishing a device we have been working on for quite awhile. I just cant get past this final problem, the problem being whenever we change screens it takes a noticeably long time for the screen…
Part Number: ESDS314 Hello TI Community,
I'm seeking advice on establishing an effective ESD protection strategy for a specific setup and would appreciate your insights. Here are the key details:
Project Overview
System Configuration : A floating…
Part Number: TPS7H2201-SP Hello,
I was wondering if you had an AVG SPICE model for the TPS7H2201-SP. If so, could you post that on the device page?
Thank you,
Zackery Painter
Slowly reduce the frequency until it regulates the output. Check the Frequency Folding technique implemented in PMP23126. This is under close loop control. Freq is gradually reduces for light load regulation. This is a released design in C2000Ware DP…
Hello, I require a low cost microcontroller/processor that supports remote Audio and Video streaming with the following added features: 1.Motion Detection 2.Night Vision 3. Mic and Speaker 4. Wi-Fi and Bluetooth 5. Camera
Part Number: SN74AC541 Hi TI Logic Team,
Do we have ch-ch skew information (of the same device) for the AC family of logic devices? Similarly to what we have for LVC family ( LVC Characterization Information )?
Thanks & BR,
KF