Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: PROCESSOR-SDK-AM57X
Tool/software:
Hi,
the recipe gstreamer1.0-plugins-hevc [1] and gstreamer1.0-plugins-vpe [2] in meta-arago cannot fetch the submodule "common". See the following example of a local clone.
$ git clone https:…
Part Number: MSP430I2041 Other Parts Discussed in Thread: TIDM-SERVER-PWR-MON Hi MSP Team,
My customer designed a single phase meter based on MSP430i2041 using TIDM-SERVER-PWR-MON as reference.
This meter has some problems.
When the USB is connected…
HI
I am very confused which one is the right gain.For the reason in TIDM-1001the PWR 050 SCH ,written that 400V=1.5V,while in another application noteTIDA-00381 that use the same PWR050SCH,that written 400V=1.96v.So please help me to make sure the right…
Hi,Paul
We're in "pull" mode
the API with the following error:
{"type":"http. ClientResponse","code":422,"headers":{"Access-Control-Allow-Headers":"*","access-control-allow-headers":"*","Access-Cont rol-Allow-Methods":"GET, POST, PUT, DELETE…
Hi Bin,
I just finished the test with a Linux PC (Ubuntu 2022.02), after a few reboots (~50), the System hang:
Log from ti am64-evm:
[ OK ] Finished File System Check on /dev/mmcblk1p1. Mounting /run/media/boot-mmcblk1p1... [ OK ] Mounted /run/media…
Alex,
These logs are difficult to analyze without context. Can you please provide the following details:
1) What application are you running? Are you running on Linux and using the native Linux display (tidss) or are you running with RTOS+Linux with an…
Hello,
The FAQ that Eddie mentioned in the thread above is still applicable if using EMDC. If that's not an option, then consider using the TIDM-SERVER-PWR-MON software based on the MSP430i2041. For the voltage and current ranges, a voltage divider…
Hi Art,
Art Mecina said: Customer have already tried to flash some default images to the EVMi2040, however after flashing the image he cannot see any results from the development board. LED indicators are working but he cannot receive any message from…