Part Number: TIDM-SERVODRIVE Other Parts Discussed in Thread: C2000WARE Tool/software: Hi,
I am programing (G code interpreter) a C2000 to control a 3D printer (currently stepper motors) I would like to use 3 x small brushless servo motors instead,…
Part Number: TIDM-SERVODRIVE Refering to TIDM-SERVODRIVE IDDK v2.2, is it possible to add external Regenerative Resistor for driving servo motor application and where to add in which of the circuit ?
Part Number: TIDM-SERVODRIVE Other Parts Discussed in Thread: CONTROLSUITE ONCE TMSF28377d'S JTAG IS ON ,SCI'S CIRCUIT IS NOT WORK? BOOT SHOULD CHOICE WHICH MODE?
Other Parts Discussed in Thread: DESIGNDRIVE , TIDM-SERVODRIVE , DRV8301 , CONTROLSUITE , TIDA-00195 Hello, both kits are based on C2000 MCU but InstaSPIN is offered up to F28069 while DesignDrive offered only with the latest and greatest F28377 MCU.…
Jason,
I was correct previously, the SDFM clocks are inputs. I checked the TIDM-SERVODRIVE schematic, and the SDFM clock inputs are driven by PWMs on the device.
Best Regards,
Ben Collier
Part Number: TMDXIDDK379D Other Parts Discussed in Thread: TIDM-SERVODRIVE Hi Team,
Customer was unable to locate the M2/M8 power supply (400V to 15V DC/DC convertrer) pcb and sch files of TMDXIDDK379D. I have provided the TIDM-SERVODRIVE design file…
Hello,
I assume you refer to the http://www.ti.com/tool/TIDM-SERVODRIVE#technicaldocuments ? In that case y ou may check for a free Gerber file viewer or editor of your choice. TI does not offers such tools.
If you however refer to the TIDA-010025…
there are several examples of using SVM on F28379,
you can definitely do this on LAUNCHXL-F2379D,
you can look at the C:\ti\controlSUITE\development_kits\TIDM-SERVO-LAUNCHXS
www.ti.com/.../TIDM-SERVODRIVE
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: TMDXIDDK379D , TIDM-SERVODRIVE , CONTROLSUITE a)is that this development kit includes TIDM servodrive inverter to control the 270VDC PMSM motor.
b)any standard test is followed to test the…
Hi Nate,
Welcome to the e2e forum! You could use the AMC1204, AMC1304 or AMC1305 for this. The clock source for the modulators would come from a PWM on your TMS320F28377S. Since the same clock would feed each modulator, there would be no problems with…