Part Number: TINA-TI Hello,
When trying to run TINA-TI Simulation I am getting this issue,
Please can you help me here.
I set the Analysis parameters to this to see if it help to resolve the issue.
Part Number: TINA-TI Hi Team,
The customer recently saw an error in TINA TI when using Bode plots. Below is a screenshot of a simple notch circuit, where it should eliminate the band at 1KHz, but it does so at 149Hz.
Can you help check and propose a possible…
Part Number: TINA-TI I'm going to purchase a new computer to run TINA-TI, what kind of computer shound I buy?
Computers with higher frequency? Or some other considerations?
Part Number: TINA-TI Other Parts Discussed in Thread: ISO6721 , ISO7721 , ISO6721-Q1 , I was trying to insert ISO6721 and ISO7721 Spice model into TINA through macro wizard tool but I was getting the following DBREAK error.
Kindly help on this. Thanks in…
Part Number: TINA-TI Other Parts Discussed in Thread: UCC2897A , Hello E2E,
I was download TINA-TI file of UCC2897A for study about forward transformer. This model has some parameters. Please tell me the meaning of each parameter.
NP1 : primary turns NS1 …
Part Number: TINA-TI Hi, i am trying to use Tina to simulate a circuit. I am trying to use the signal analyzer to display the total harmonic distortion. I have been watching a tutorial on a youtube channel called TinaDesignSuite, and they have an option…
Part Number: INA240 Hi Expert,
I'm using below circuits to simulation with INA240A4.
The input is 10mV, 320kHz half- sinusoidal signal, however the output is very weird. There are mainly 2 issues:1). the valley value of out put signal is too far from…
Part Number: TINA-TI Hi team,
There is an error occurs when i import new macro wizard from SPICE model.
ad8641 (1).cir
could you kindly help on this?
Thanks a lot
Matthew
Part Number: OPA1677 Other Parts Discussed in Thread: TINA-TI The data sheet for the OPA1677 shows a schematic (see Fig 8-1) for a Phantom powered preamp designed for a piezo transducer mic. It states that a TINA-TI simulation of the circuit is available…
Part Number: TLV767-Q1 Other Parts Discussed in Thread: TINA-TI Hi team,
Do you have TINA-TI transient model including 1/f noise characteristics?
Regards, Ochi