Part Number: TIOL1115EVM Other Parts Discussed in Thread: TIOL1115 I powered up the EVM board via the IO-Link master and the following LED's show up:
D1 : VCC in/out is on
D2: NFault is off
D3: Wake is faint orange led
D4: L+ is off although L…
Part Number: TIOL1115EVM Hello all,
I am working on developing an IO-Link device with the TIOL1115EVM.
With the evaluation board, i am not using the VCC out of this.
Is it necessary for me to connect the Enable via pull down resistors, wake via…
Part Number: TIOL1115EVM Other Parts Discussed in Thread: TIOL1115 , TIOL1113
Hello,
The pins on the TIOL1115EVM are connected to the STM32 Microcontroller as following:
Enable pin as output pin with internal pull down resistor
Wake pin, and Nfault…
Part Number: TIOL1115EVM Hello Team,
My customer is looking for the physical dimensions, preferable a 2D dwg., of the TIOL1115EVM. To include fastener hole locations for design and installation.
Regards,
Renan
Part Number: TIOL1115EVM Other Parts Discussed in Thread: TIOL1113 , TIOL111 , TIOL1115 Hello,
I have a TIOL1115EVM board, which i'm trying to connect to an Arduino using UART.
GROUND, TX, and RX are connected to the Arduino pins. Ground on ground…
Hi Mira,
What is the voltage level you are applying on L+ ? Also, you said you are concerned with the L+ voltage level because you are using the internal 5V LDO to supply your MCU. Have you monitored the 5V for any variation when CQ switches? I am not…
Part Number: TIOL1115EVM I think i have connected the L+ and L- wires wrongly with the CQ line and due to which the Nfault LED is always on and the VCC out is only giving me 2.4V instead of 5V.
All the other LED's are now very dim as compared to earlier…
Hello Pulla,
For the SN65HVD101 I would recommend referencing Figure 11 in the datasheet for an implementation schematic. For TIOL111, you could reference Figure 17. Both devices also have EVMs available that could be used as an example (although a…
Hi Venkatesh,
the SN65HVD101EVM and the TIOL1115EVM both are generic EVMs that that only contain the IO-Link transceiver and can be connected to any microcontroller board of your choosing. Therefore there is no firmware provided with these EVMs and…