Hi John,
Take a look at the DAC8760, or a DAC + XTR combination like the design shown in TIPD155 .
We also have a few reference designs featuring the DAC8760. Take a look at TIPD119 and TIPD153 .
Hello Luke,
The XTR300EVM is an evaluation platform only and should not be used in a final product. This is stated in the information placed with the EVM.
The XTR300 is the product featured in the XTR300EVM and is a great choice for your design. It is…
Hello Hawk,
Please take a look at TIPD155:
It is a reference design that showcases the DAC8562 and two XTR300s for a dual-channel analog output module that can source and sink voltage and current.
Please let us know if you have any questions about this…
Hello Christoph,
If a voltage is applied to the inputs or outputs of the XTR300 that is greater than the power supply voltages, the internal ESD protection diodes will conduct. Current should not exceed 10mA through the protection diodes. It is best if…
Hi David,
Could you send let us know the input / output ranges of your system? Also provide a schematic and a few scope captures of the following signals:
1.) XTR300 output 2.) V+ 3.) V- 4.) GND
Please ac couple the scope inputs and zoom in so we can observe the…
Other Parts Discussed in Thread: PGA309 , TIPD126 , TIPD153 , TIPD155 Hello
our pressure transmitter are mainly formed by your PGA309 programmable conditioner and power supply chip TPS7A41. in order to pass electrically fast transient test, we add some ferrite…
Hi Ignacio,
I'm not quite sure what you are asking. The simulation is not going to reflect the true accuracy of the XTR300 in voltage output mode. The true output should be closer to that predicted by the equations than what is shown in sim. The dominant…
Hi Johan,
Johan Bergman said:
For me to be able to start recording the geophone data and to do this with a minimum of modification to the ADS1282EVM-PDK have I understood you correctly that by only adding the R5 and R6 resistors to the J6 header as we have…