Part Number: TL074-EP Other Parts Discussed in Thread: TL074 , , TL074H , OPA4991-EP Tool/software: Hello Team,
Here is the analog output application with TL074QDREP in motor drive. The bias supply of TL074QDREP is 0V(VCC-) and 15V(VCC+). With this…
Part Number: TL074-EP Other Parts Discussed in Thread: TL074 Tool/software: In the TL07xH d/s, it specifics the short-circuit current as +/-26mA. However, we don't see it for TL074QDREP?
Could you help on this!
Regards
Brian
Part Number: TL074-EP Other Parts Discussed in Thread: TINA-TI , TL074 , OPA1644 What are the output impedance for TL074IDR、TL074QDREP and TL074QDREPA?
Customer would like to do the simulation with this ZO! please help. thanks.
Regards
Brian
Other Parts Discussed in Thread: TL074 , LM148 , LT1014A , TLE2074M Hi,
I see there is an EP version of the TL074 but it only operates down to -40c. Is this correct - I thought all EP parts went to -55?
Is there an alternate to the tl074 that will…
The TL074-EP datasheet specifies some characteristics for a range between 10 V and 30 V.
Both the TL074-EP and the TL074H allow an output to be shorted with unlimited duration. The TL074-EP datasheet does not specify what current flows in that case;…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…