Part Number: TL074 Other Parts Discussed in Thread: TL081H Tool/software: A problem occurred where several TL074IDRs oscillated.
I'm investigating whether EOS is the cause, or if there is a problem with the circuit and the oscillation is caused by variations…
Part Number: LM2904V Other Parts Discussed in Thread: OPA990 , TL081H , INA180 Tool/software: Hi TI,
I use LM2904V to design a high side current sense circuit.
I hand made a circuit and measure it, but output voltage is abnormal at Vbat lower than…
Part Number: LMV358A Other Parts Discussed in Thread: TLV9001 , TL081H , , LMV358 , LMV321 The following figure is used for current limiter. In normal, load current is small. VIN + is 4V . VIN- is greater than 4V, which exceeds Common-mode voltage range…
Part Number: LM2904 Other Parts Discussed in Thread: TL071H , TL081H
您好
請問使用LM2904 使當電流琛偵測使用 RS= 15m 歐姆
R1=R3=1.1K
R2=R4= 100K
vo 理論上會是多少呢?
我從電表或示波器上看到都在12.8~13.3 v 這是合理的嗎? 還是已經進入飽和呢?
Part Number: LF411 Other Parts Discussed in Thread: TL071H , TL081H Hello team,
My customer is simulating a circuit based on SBOA436( https://www.ti.com/lit/an/sboa436/sboa436.pdf ).
In the simulation, we obtained an output clip of current and voltage…
Part Number: TL071H Other Parts Discussed in Thread: TL081H Please let me know,
1. What is the difference between TL071H and TL081H? How to choose in applications?
2. In a single 12Vcc application, VIN+ = 3V and VIN- = 2.5V, w hat will happen to the…
Part Number: TL084A Other Parts Discussed in Thread: TL084 , TL081H , TL084H Hi,
Hi, To what current, if any, would the attached current clamp regulate the current, given that it is being operated outside of its common mode input range? LTspice and…
The new die is identical with the TL081H and uses a different architecture, so the same offset adjustment mechanism is no longer possible. As far as I know, these pins are NC.
Pins 2 and 6 are IN− and OUT. A diode between these pins would prevent the amplifier from working correctly.
Anyway, PCN# 20220615003.1 introduced a new die; it is now identical with the TL081H.
Part Number: OPA170 Other Parts Discussed in Thread: TLV9101 , OPA990 , TL081H
Hi, this is my new thread in relation of my other thread ( OPA170 Abnormal Behaviour ).
My setup (use as current sensor : V2 connecting V3 with ~0.1 ohm;150C test)
V1…