Part Number: TL082H Other Parts Discussed in Thread: TL082 , Tool/software: The TL082H has a compelling price to performance ratio, far improved common mode range and rail to rail outputs over the old TL082.
All looks very good until I find no mention…
Part Number: TL082H Other Parts Discussed in Thread: TL032 , Hi,
My customer considers to replace from TL032 to TL082H.
On both datasheet, In: Equivalent input noise current (f=1KHz) is different between 0.003pA/ √ Hz on TL032 and 0.080pA/ √ Hz on…
Part Number: TL082H Other Parts Discussed in Thread: TL082 Hi Team
As the datasheet shows, input voltage range is Vcc-+2V.Can I understand that when the reverse pin(VF1) is lower than the voltage value, TL082H will work abnormally or even fail.
Part Number: TL082H Other Parts Discussed in Thread: TL082 , Hi team,
Could you give me comment on why the supply voltage specification description is different between TL08x and TL08xH like below? It's not sure if this difference suggests different…
Part Number: TIDA-00555 Other Parts Discussed in Thread: TMDSCNCD28P65X , TL082H , TMDSHSECDOCK Tool/software: Looking for voltage and current measurement evaluation boards (not IC chip only such as TL082H that requires soldering). I already bought one…
Part Number: TL062 Other Parts Discussed in Thread: TL072H , TL082H , OPA2990 , LM358B , Hey team,
I'm trying to recommend a replacement for the TL062CPWR because my customer wants to move to a MSOP package for supply chain reasons. I found the TL072H…
Hi Zoey,
Clemens Ladisch said: There was no PCN for the TL082H.
The record is shown the TL082H is in RFAB, and PCN is related to 20230627002 series. The reason the part does not have PCN is that TL082H is designed in RFAB first; then use it as the…
Hi Ashley:
I explain about this case.
1. The customer's current mass-produced flow meter products use TI's TL082, and the solution is very stable and has been in mass production for nearly 7 or 8 years. 2. The customer had previously considered iterating…
Hi Lei,
If the supply is +/-5V then the input signal would need to adhere to the input linear common mode voltage range which is typically Vee+3V and to Vcc. The linear output swing is approximately 1.5V-3V within the supply rail for the old device…