Part Number: TIDA-00555 Other Parts Discussed in Thread: TMDSCNCD28P65X , TL082H , TMDSHSECDOCK Tool/software: Looking for voltage and current measurement evaluation boards (not IC chip only such as TL082H that requires soldering). I already bought one…
Part Number: TL062 Other Parts Discussed in Thread: TL072H , TL082H , OPA2990 , LM358B , Hey team,
I'm trying to recommend a replacement for the TL062CPWR because my customer wants to move to a MSOP package for supply chain reasons. I found the TL072H and…
Below the minimum recommended supply voltage of 4.5 V, correct operation is not guaranteed.
Try the TL082H, which has a different architecture, but no such amplifer guarantees the behaviour of the output with an invalid supply. You would have to use opamp…
With a 12 V supply, the drive strength should be similar.
Figure 6-44 shows that the output voltage range depends mainly on the load.
I would strongly suggest the more modern TL082H, which is cheaper and has rail-to-rail outputs.
Hey Maggie,
There are a couple changes you can make to see the stability of this circuit, however the TL082 model is fairly outdated and may not accurately model stability.
There is a newer version of this device, the TL082H, which I will use for this…
Hello Calvin
I suspect that this is a parasitic path that is capacitance and resistance in series.
I suggest added and input low pass filter to slow the input signal. Or use TL082H that doesn't have this direct path.
Hi Dylan,
it's essentially the same. Often (but not always) "Aol" is specified without load resistance and "Avd" is specified with defined load resistance.
Keep in mind, that the datasheet contains two totally different OPAmps…
Hi Kai
Thanks a lot for your detail answer. Yes, because TL082H is not a rail to rail input amps, so I replace TL082H by TLV9352 which has better performance. The diode in fact is a Mosfet, for easy to understand so I replace it by a diode. Of course…
Part Number: OPA2145 Other Parts Discussed in Thread: LF412 , , TL082H , LOG114 , TL072 , OPA397 , OPA392 , OPA197 , OPA192 , LMP7721 , OPA828 , OPA2392 , LMP2012 Hi Experts,
We are working on a solution with log amplifier and thinking of developing a circuit based…